This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运行的Pa_emacExample结果



请问 我在6678上运行的Pa_emacExample结果运行对吗?这能说明硬件的sgmii mavel部分是没问题的吗?运行整个流程是怎样的?请帮忙解答一下 谢谢

[C66xx_0] **************************************************

[C66xx_0] ******* Ethernet Single Core Example Start *******

[C66xx_0] **************************************************

[C66xx_0] QMSS successfully initialized

[C66xx_0] CPPI successfully initialized

[C66xx_0] PASS successfully initialized

[C66xx_0] Ethernet subsystem successfully initialized

[C66xx_0] Tx setup successfully done

[C66xx_0] Rx setup successfully done

[C66xx_0] PASS setup successfully done

[C66xx_0] Following is the ALE table before transmits.

[C66xx_0] Port = 0, MAC address = 10:11:12:13:14:15, unicast_type = 0

[C66xx_0] Port = 1, MAC address = 10:11:12:13:14:15, unicast_type = 0

[C66xx_0] Port = 2, MAC address = 20:21:22:23:24:25, unicast_type = 0

[C66xx_0] Packet Transmission Start ...

[C66xx_0] Following is the ALE table after transmits.

[C66xx_0] Port = 0, MAC address = 10:11:12:13:14:15, unicast_type = 0

[C66xx_0] Port = 1, MAC address = 10:11:12:13:14:15, unicast_type = 0

[C66xx_0] Port = 2, MAC address = 20:21:22:23:24:25, unicast_type = 0

[C66xx_0] Packet Transmission Done.

[C66xx_0] Wait for all packets to be Received ...

[C66xx_0] Packets Sent = 10

[C66xx_0] Packets Received = 10

[C66xx_0] Example Done!

[C66xx_0] **************************************************

[C66xx_0] ******** Ethernet Single Core Example End ********

[C66xx_0] **************************************************