各位大神好,
最近刚用am335x的芯片,下载 ti-processor-sdk-linux-am335x-evm-02.00.02.11-Linux-x86-Install.bin ,在虚拟机上运行Ubuntu9.10,安装不了sdk,显示 cannot execute binary file 为什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大神好,
最近刚用am335x的芯片,下载 ti-processor-sdk-linux-am335x-evm-02.00.02.11-Linux-x86-Install.bin ,在虚拟机上运行Ubuntu9.10,安装不了sdk,显示 cannot execute binary file 为什么呢?
我下载了ubuntukylin-14.04.1-desktop-i386.iso ,在虚拟机安装了,但是还是不行bash: ./ti-processor-sdk-linux-am335x-evm-02.00.02.11-Linux-x86-Install.bin: cannot execute binary file: Exec format error,看到TI说If nothing seems to happen, you are probably running a 32-bit version of Linux. The installer is 64-bit, and will not execute properly. 这个意思是说要安装64bit的Ubuntu吗? 去下载ubuntukylin-16.10-enhanced-amd64.iso 用vm安装不了 到底怎么回事?
可以参考下面的链接,
http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Getting_Started_Guide
看你的描述这里:
我电脑是64bit的,安装的虚拟机是vm12,安装64的amd linux不成功,安装32位linux后bin文件打不开
你的ubuntu是多少位的和你的电脑主机无关,所以即使你目前电脑是64位的,但是装的是32位Linux也是白搭,还是跑不了。
可以按照下面的连接中给出的资源地址,下载相关的image,来进行操作,这个是肯定没问题的。
http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Getting_Started_Guide#Start_your_Linux_Development