运行所有的OpenCL例子的时候出现了如下的错误:
TIOCL FATAL: OpenCL needs 1 CMEM blocks to operate - one each for off-chip (DDR) and on-chip (MSMC SRAM or OCMC RAM) memory
求指点迷津!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
运行所有的OpenCL例子的时候出现了如下的错误:
TIOCL FATAL: OpenCL needs 1 CMEM blocks to operate - one each for off-chip (DDR) and on-chip (MSMC SRAM or OCMC RAM) memory
求指点迷津!!!
--- a/arch/arm/boot/dts/am57xx-beagle-x15-common.dtsi
+++ b/arch/arm/boot/dts/am57xx-beagle-x15-common.dtsi
@@ -62,6 +62,18 @@
reusable;
status = "okay";
};
+
+ cmem_block_mem_0: cmem_block_mem@a0000000 {
+ reg = <0x0 0xa0000000 0x0 0x0c000000>;
+ no-map;
+ status = "okay";
+ };
+
+ cmem_block_mem_1_ocmc3: cmem_block_mem@40500000 {
+ reg = <0x0 0x40500000 0x0 0x100000>;
+ no-map;
+ status = "okay";
+ };
};
vdd_3v3: fixedregulator-vdd_3v3 {
@@ -93,6 +105,27 @@
gpio = <&gpio7 11 GPIO_ACTIVE_HIGH>;
};
+ cmem {
+ compatible = "ti,cmem";
+ #address-cells = <1>;
+ #size-cells = <0>;
+
+ #pool-size-cells = <2>;
+
+ status = "okay";
+
+ cmem_block_0: cmem_block@0 {
+ reg = <0>;
+ memory-region = <&cmem_block_mem_0>;
+ cmem-buf-pools = <1 0x0 0x0c000000>;
+ };
+
+ cmem_block_1: cmem_block@1 {
+ reg = <1>;
+ memory-region = <&cmem_block_mem_1_ocmc3>;
+ };
+ };
+