This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
stareware 库的usblib.h文件的注释中出现的
//! The standard USB request header as defined in section 9.3 of the USB 2.0
//! specification.
和// Definitions related to USB descriptors (sections 9.5 & 9.6)
中的section 9.3 of USB2.0 specation 和 USB descriptors (sections 9.5 & 9.6) 指的是什么,在哪里?
没看明白,求解。
starterware 库有USBlib 库,我看了例程,库里面有usbdbulk.c和usbdbulk.h 关于bulk传输的文件。
关于USB device 控制传输的例程和文件在哪里???
starterware库的usblib中的usbdata.c 中 有定义tUSBInstanceObject g_USBInstance[USB_NUM_INSTANCE]; USB_NUM_INSTANCE = (1);
也就是定义了g_USBInstance[1];
在 device 文件中的 USB1DeviceIntHandler(void)函数中却出现了 ulStatus = HWREG(g_USBInstance[1].uiSubBaseAddr + USB_0_INTR_SRC);
出现了g_USBInstance[1] 变量,定义时结构体数组g_USBInstance[]只有一个成员,怎么会出现g_USBInstance[1].uiSubBaseAddr那?