使用的am335x,现在已经可以用EDMA读GPMC数据,但每次都是使用的edma_start()来启动DMA,请问如何使用GPIO触发EDMA自动读取GPMC数据。
edma和gpmc的配置如下:
static int gpmc_config(void)
{
int error;
u32 val;
int cnt;
// Chip-select configurations
val = gpmc_cs_read_reg(GPMC_FPGA_CS, GPMC_CS_CONFIG7);
val &= ~GPMC_CONFIG7_CSVALID; /*disable chip-select*/
gpmc_cs_write_reg(GPMC_FPGA_CS, GPMC_CS_CONFIG7, val);
gpmc_cs_configure(GPMC_FPGA_CS, GPMC_SET_IRQ_STATUS, 0); /*set irq status*/
gpmc_cs_configure(GPMC_FPGA_CS, GPMC_ENABLE_IRQ, 0); /*disable irqs*/
// Config NOR Memory Type
gpmc_cs_write_reg(GPMC_FPGA_CS,GPMC_CS_CONFIG1, GPMC_CONFIG1_READTYPE_ASYNC | /*set read type Asynchronous*/
GPMC_CONFIG1_WRITETYPE_ASYNC | /*set write type Asynchronous*/
GPMC_CONFIG1_DEVICESIZE_16 | /*set device size 16bit*/
GPMC_CONFIG1_DEVICETYPE_NOR | /*set device type NOR*/
GPMC_CONFIG1_FCLK_DIV3); /*GPMC_CLK frequency=GPMC_FCLK frequency/3*/
// Non-mutiplexed Address and Data
val = gpmc_cs_read_reg(GPMC_FPGA_CS, GPMC_CS_CONFIG1);
val &= ~GPMC_CONFIG1_MUXADDDATA; /*Non-multiplexed attached device*/
gpmc_cs_write_reg(GPMC_FPGA_CS, GPMC_CS_CONFIG1, val);
//GPMC Timing parameters
error = gpmc_cs_set_timings(GPMC_FPGA_CS, &fpga_timings); /*set timing parameters*/
if(error < 0){
DPRINTK(KERN_ERR "Unable to set gpmc timings\n");
return error;
}
/***********为FIFO申请GPMC chip-select空间**********/
if (gpmc_cs_request(GPMC_FPGA_CS, GPMC_FIFO_SIZE, &gpmc_membase)<0)
{
DPRINTK(KERN_ERR "gpmc_cs_request failed.\n");
return -1;
}
return error;
}
static int edma_config(void)
{
int result = 0;
unsigned int BRCnt = 0;
int srcbidx = 0;
int desbidx = 0;
int srccidx = 0;
int descidx = 0;
struct edmacc_param param_set;
/* Set B count reload as B count. */
BRCnt = bcnt;
/* Setting up the SRC/DES Index */
srcbidx = 0;
desbidx = acnt;
/* A Sync Transfer Mode */
srccidx = 0;
descidx = acnt;
result = edma_alloc_channel (52, callback1, NULL, EVENTQ_0);
if (result < 0) {
DPRINTK ("edma_config::edma_alloc_channel ""failed for dma_ch1, error:%d\n", result);
return result;
}
dma_ch1 = result;
edma_set_src (dma_ch1, (unsigned long)(gpmc_membase), INCR, W16BIT);
edma_set_dest (dma_ch1, (unsigned long)(dmaphysdest1), INCR, W16BIT);
edma_set_src_index (dma_ch1, srcbidx, srccidx);
edma_set_dest_index (dma_ch1, desbidx, descidx);
edma_set_transfer_params (dma_ch1, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 1 */
edma_read_slot (dma_ch1, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch1));
edma_write_slot(dma_ch1, ¶m_set);
/* Request a Link Channel */
result = edma_alloc_slot (0, 64);
if (result < 0) {
DPRINTK ("edma_config::edma_alloc_channel ""failed for dma_ch2, error:%d\n", result);
edma_free_channel(dma_ch1);
return result;
}
DPRINTK ("edma_config::edma_alloc_channel ""success for dma_ch2, dma_ch2:%d\n", result);
dma_ch2 = result;
edma_set_src (dma_ch2, (unsigned long)(gpmc_membase), INCR, W16BIT);
edma_set_dest (dma_ch2, (unsigned long)(dmaphysdest2), INCR, W16BIT);
edma_set_src_index (dma_ch2, srcbidx, srccidx);
edma_set_dest_index (dma_ch2, desbidx, descidx);
edma_set_transfer_params (dma_ch2, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 2 */
edma_read_slot (dma_ch2, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch1));
edma_write_slot(dma_ch2, ¶m_set);
/* Link both the channels */
edma_link(dma_ch1, dma_ch2);
/* Request a Link Channel */
result = edma_alloc_slot (0, 65);
if (result < 0) {
DPRINTK ("edma_config::edma_alloc_channel ""failed for dma_ch3, error:%d\n", result);
edma_free_channel(dma_ch1);
edma_free_slot(dma_ch2);
edma_free_channel(dma_ch2);
return result;
}
DPRINTK ("edma_config::edma_alloc_channel ""success for dma_ch2, dma_ch2:%d\n", result);
dma_ch3 = result;
edma_set_src (dma_ch3, (unsigned long)(gpmc_membase), INCR, W16BIT);
edma_set_dest (dma_ch3, (unsigned long)(dmaphysdest1), INCR, W16BIT);
edma_set_src_index (dma_ch3, srcbidx, srccidx);
edma_set_dest_index (dma_ch3, desbidx, descidx);
edma_set_transfer_params (dma_ch3, acnt, bcnt, ccnt, BRCnt, ASYNC);
/* Enable the Interrupts on Channel 2 */
edma_read_slot (dma_ch3, ¶m_set);
param_set.opt |= (1 << ITCINTEN_SHIFT);
param_set.opt |= (1 << TCINTEN_SHIFT);
param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(dma_ch1));
edma_write_slot(dma_ch3, ¶m_set);
/* Link both the channels */
edma_link(dma_ch2, dma_ch3);
edma_link(dma_ch3, dma_ch2);
return 0;
}