This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148/DM8127的BT.1120接口问题



  • 1、完全采用TI DM8127 EVB板参考电路,不做任何更改和调整。仅仅更换SENSOR board(MT9J003)部分。SENSOR board(MT9J003)更换为另一颗SENSOR。这颗SENSOR是标准的BT.1120输出,有Y7-Y0,C7-C0数据线16条。而MT9J003只使用了12条数据线。请问,如果我们把更换后的SENSOR 的BT.1120的输出直接接入DM8127的BT.1120 (原来接MT9J003的接口),是否可行?软件上除了更换SENSOR的driver,其它部分的软件参数是否需要调整?

    2、SENSOR board(MT9J003)参考电路如只接了12条数据线、H、V行、场同步线、CLK、I2C。而我们所更换的SENSOR是BT.110输出,有16条数据线、CLK、I2C、无行、场同步信号,请问,DM8127通过这样的连接方式连接到这颗SENSOR是否有问题?

    3、我查过DM814X的资料,其BT.1120输入接口如下所示:

    VIN[0]A_(D7-D0)   Cb/Cr(AA11、AH16、AG16、AH8、AE12、AC9、AB11、AF9)

    VIN[0]A_(D15—D8) Y(AC14、AC12、AF17、AG17、AH17、AH9、AG9、AB15)

    VIN[0]A_HSYNC  (AF21)

    VIN[0]A_VSYNC  (AD20)

    VIN[0]A_CLK     (AB20)

    这个BT.1120 输入的数据线、CLK与现在EVB板DM8127的参考设计不同,请问我们连接SENSOR时是否需要接入这个接口?