This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678EVM板,存储器吞吐量测试比STK中文档里介绍的速率慢很多



硬件环境:6678EVM板

软件环境:不使用系统

        使用6678的EVM板的两个版本——Rev1.0和Rev.3B,对STK例程包中的memory performance例程进行测试时,发现使用DSP核访问LL2、SL2、DDR的速率,比起STK中doc文件夹里文档说明的要低得多。

        比如文档里DSP核对L1与L2之间、L2与DDR之间、SL2与DDR之间、DDR与DDR之间的通信速率都能达到1GB/s甚至2GB/s,可是我在两个版本的EVM板上运行这个例程,速率只能达到几十MB/s到几百MB/s,远低于文档里的测试结果。

       请问TI的工程师,STK文档里的测试结果是在哪一个芯片型号及EVM板型号上运行得到的?我的测试结果这么低会是什么原因?程序是直接在论坛里下到的K1_STK_V1.1.

      不知道各位有没有测试过这个例程,跟我的测试结果类似吗,谢谢