ti'er,
采用git上最新的uboot DVO2和HDMI能同时输出分辨率为1920*1080的logo,SD输出的不是logo图像,怎么修改才能让SD也能输出logo图像呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ti'er,
采用git上最新的uboot DVO2和HDMI能同时输出分辨率为1920*1080的logo,SD输出的不是logo图像,怎么修改才能让SD也能输出logo图像呢?
Li Xiaobo,
SD输入的分辨率是D1,而你logo的大小是1080p,当然无法直接输出。
Chris Meng ,你好
恩,图像大小是不一致。但是像应用程序显示效果一样处理,有两种显示方式:
1.用缩放模块,和应用层类似,缩放后再显示。
2.直接显示logo的中间部分,我们logo图像中间会有公司logo,边沿部分不显示。
Li Xiaobo,
你的意思是SD上可以显示缩小的1080p的图,但是图像比较暗?
我看了一下uboot logo的代码,利用的是GRPX作为显示层显示logo的。GRPX硬件本身是支持缩放的。
Chris Meng,
你是说HDMI和DVO2都按照1080P的显示,但是BMP图只给640x480这样吗? 这种情况下SD也是不能正常显示,HDMI和DVO2能正常显示,logo图在中间。