Hi:
tms320c6748使用fatfs文件系统读写SD卡,读写4g,8g,16g,32g都是可以的,但是读写 64g以上的SD卡会出现错误。
是因为fatfs文件系统的原因吗?如果需要换文件系统,应该换哪一种?
Ti关于这一方面问题的文档在哪里?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
tms320c6748使用fatfs文件系统读写SD卡,读写4g,8g,16g,32g都是可以的,但是读写 64g以上的SD卡会出现错误。
是因为fatfs文件系统的原因吗?如果需要换文件系统,应该换哪一种?
Ti关于这一方面问题的文档在哪里?
谢谢!
看看是不是SD卡的标准
6748支持
The device includes an two MMCSD controllers which are compliant with MMC V4.0, Secure Digital Part 1
Physical Layer Specification V1.1 and Secure Digital Input Output (SDIO) V2.0 specifications.