我现在用两个核在BIOS模式下,核1使用EDMACC1的通道1,核2使用EDMACC1的通道2;我看了大多数的例子就是核触发EDMA传输,之后一直查看IPR对应位的数值,当EDMA传输完成的时候,对应的IPR的第二位和第三位会置1;我现在是想利用中断,当核1的传输完了之后IPR置1,之后让核1中断去清零IPR,同样的当核2传输完成之后,IPR的对应位置1,触发核2中断,去清除IPR位;因为在两个核,但是他们用的是同一个EDMACC,不知道怎么把两个中断分开,看了很长一段时间中断那一块,对于EDMA传输完成中断还是没弄懂??如果TI有这种例子的话,那是最好啦