This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM368解码的问题



hi:

我们这套系统前端采集的是720p的图像,压缩编码都没有问题,但是我们采用标清(BT656)解码时出现了一些小状况

我想问几个问题:

1、高清录像,标清解码是否可行

2、若可行,图像会是scaler还是截取其中的一部分?

  • BT656是数字输入或者输出口的协议,和解码有什么关系?

  • hi Meng

    BT656是标清的啊,我想问一下高清编码,标清解码是否会有问题,另外,如果可以的话,他的输出是scaler的还是从高清中截取的?(因为高清是16:9,标清是4:3)

  • Lv Xianmin,

    你能再解释一下你说的标清解码是什么意思么?

    是使用DM368解码D1分辨率的码流?还是通过VPBE输出BT656的信号?

  • Dear Chris Meng,

    我们的应用是这样,dm368,vpfe高清采集,720P编码保存264文件。然后可以通过dm368本地解码264文件,通过vpbe输出BT656信号到外部监视器。

    保存的.264视频文件是通过dvsdk-demo的encode保存的,720P25。

    然后通过dvsdk-demo的decode 来解码这个720P25的.264文件,但解码时使用的是-y2(PAL)做标清解码。解出来看到的图像边缘有些异常。

    我们想咨询一下,这种使用方式是否会有问题?高清编码后,标清解码是对原始的16:9图像怎样处理后变成4:3的?

    谢谢!


  • Lv Xianmin,

    下面的信息是在decode.txt里面摘抄的:

           -y <1-3>, --display_standard <1-3>
                 Sets the resolution of the display. Clips larger than the display
                 will be center clamped, and clips smaller than the display will
                 be centered.

                        1       D1 @ 30 fps (NTSC) [Default]
                        2       D1 @ 25 fps (PAL)
                        3       720P @ 60 fps