This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDCTools 工具版本差异

在链接:software-dl.ti.com/.../index_FDS.html下载xdctool时,发现有两个版本:

1 3.31.01.33 Core (Windows)               3.31.01.33 Core for Windows

2 3.31.01.33 Core - JRE (Windows)    3.31.01.33 Core without a JRE for Windows

两者的区别是什么?在具体安装时怎么选取合适的版本?


 

  • 一般来说相应的软件包对XDC版本要求是有说明的,根据软件包的要求选择安装相应版本就行。你也可以装多个版本,用的时候选择相应版本就行了。

  • 看了doc内的描述:

    • XDCtools Core: the default release that does not include any embedded targets or platforms. This release is 100% self contained and can be used in virtually any development environment: standalone command line based environments as well as in non-Java based GUI IDEs.
    • XDCtools Core - JRE: the same as XDCtools Core but without an included Java Runtime Environment (JRE). This bundle is significantly smaller but, in order to use this release at the command line, it also requires the user to set the environment variable XDCTOOLS_JAVA_HOME to the installation directory of either an existing JRE or Java Developers Kit (JDK).