This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问6678全局定时器用法

Other Parts Discussed in Thread: SYSBIOS

硬件环境:TI 6678EVM

需求:记录core0和core1产生的计算数据时,为了对比多核间产生数据的先后,要用一个全局计时器来记录时间。

此工程是一个未使用SYS/BIOS的工程,因此需要自己构建全局计时器,不调用SYSBIOS模式下的计时器API函数。

从手册上看到,Timer8-Timer15是8个核都能访问的全局计时器,这是不是意味着core0和core1如果使用全局计时器,就相当于以同一个时间轴为标准。

如果使用这个全局计时器,core0和core1是否都需要对全局计时器进行一些初始化工作,还是只需要core0初始化完成后,core1也能正常访问该定时器。

如果core0和core1同时使用这个全局计时器,这个全局计时器要配置成什么模式。读计数的时候是什么方式。

如果能提供多个核使用一个全局计时器的范例程序就太好了。

期待回复,感谢!