我在尝试使用IAR编译AM335X_StarterWare_02_00_01_01工程中的示例程序,参照方法为:http://bbs.21ic.com/icview-757324-1-1.html
我调用的是AM335X_StarterWare_02_00_01_01中的gpio工程,先把库编译了一遍,然后直接打开工程进行编译,并通过了编译。通过J-LINK进行下载调试连接图如下:
(1).目前在IAR软件中,可以将程序下载进开发板中,并进入调试界面,但是GPIO灯并不闪烁。并出现了如下的调试错误,请问该如何修改配置。
(2).同时执行gpio例程程序。在main函数中有while(),全速运行可以进入while(),如下图,但是高低电平设置灯不亮。而且全速运行只执行了一个周期,即不能在while中循环。