This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x_EVM Uboot启动问题

Other Parts Discussed in Thread: AM3359, TMDXEVM3358

求助:

         最近使用TI的官方开发板进行Linux开发,用的SDK版本是ti-processor-sdk-linux-am335x-evm-03.02.00.05-Linux-x86。

         按照官方指导制作了SD卡,SD卡容量是8GB,启动时出现以下问题,请问应该怎么解决啊。

U-Boot SPL 2016.05 (Dec 22 2016 - 18:36:44)

Trying to boot from MMC1

reading args

spl_load_image_fat_os: error reading image args, err - -1

reading u-boot.img

reading u-boot.img

reading u-boot.img

reading u-boot.img

U-Boot 2016.05 (Dec 22 2016 - 18:25:44 +0800)

CPU : AM335X-GP rev 1.0

Model: TI AM335x EVM

Watchdog enabled

DRAM: 512 MiB

NAND: 0 MiB

MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1

MMC: no card present

** Bad device mmc 0 **

Using default environment

<ethaddr> not set. Validating first E-fuse MAC

Net: eth0: ethernet@4a100000

Warning: usb_ether MAC addresses don't match:

Address in SROM is de:ad:be:ef:00:01

Address in environment is d4:94:a1:52:3f:73

, eth1: usb_ether

Press SPACE to abort autoboot in 2 seconds

MMC: no card present

MMC: no card present

MMC: no card present

MMC: no card present

MMC: no card present

data abort

pc : [<9ff70480>] lr : [<9ff6f681>]

reloc pc : [<8081e480>] lr : [<8081d681>]

sp : 9ef27678 ip : 9ff57c31 fp : 00000003

r10: 9ffb3208 r9 : 9ef31ed8 r8 : 9ef3bf90

r7 : 9ff577b9 r6 : 9ef33630 r5 : 9ef336b8 r4 : 47810000

r3 : 9ff70471 r2 : 00000c0f r1 : 9ffa4e31 r0 : 9ef336b8

Flags: nZCv IRQs off FIQs on Mode SVC_32

Resetting CPU ...

resetting ...

  • 你用的是哪个开发板?从log上看,MMC没有正常识别。你是用的create sd脚本来做的启动SD卡吗?

  • 您好,是AM3359的一快开发板,用create sd脚本做的SD卡,我看了下代码,uboot里判断了SD卡cd引脚状态,这个状态的判断好像有问题。


    int mmc_start_init(struct mmc *mmc)
    {
        int err;
        int uhs_en = true;

        /* we pretend there's no card when init is NULL */
        if (mmc_getcd(mmc) == 0 || mmc->cfg->ops->init == NULL) {
            mmc->has_init = 0;
    #if !defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_LIBCOMMON_SUPPORT)
            printf("MMC: no card present\n");
    #endif
            return NO_CARD_ERR;
        }

        if (mmc->has_init)
            return 0;

  • 用的是这一款开发板:http://www.ti.com.cn/tool/cn/tmdxevm3358?keyMatch=am335x%20evm&tisearch=Search-CN-Everything

  • 这个是我们的官方的GPEVM板,PDK中不需要做任何的改动就可以正常使用才对。

    不排除你的板子上硬件有问题,我能想到的一个最快辨别的方法就是用串口启动,导入spl和uboot,然后在uboot中尝试读取你的SD卡内容,看看能否正常读取成功。你试试看这样做的结果怎样。