This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何搜索C6416的开发例程



您好,我想问一下,怎么在官方网站找到C6416的例程?之前找28335的很容易,但是6416的就是没找到,还请帮帮忙~非常感谢您!

  • 可以参考一下这里面的例程:

    http://www.ti.com/tool/sprc090

    DescriptionThe Chip Support Library (CSL) provides an application programming interface (API) used for configuring and controlling the DSP on-chip peripherals for ease of use, compatibility between various C6000 devices and hardware abstraction. This will shorten development time by providing standardization and portability. The functions listed in the features section are specifically designed for the following devices: C6201, C6202, C6203, C6204, C6205, C6211, C6410, C6412, C6413, C6414, C6415, C6416, C6418, C6701, C6711, C6712, C6713, DA610, DM640, DM641 and DM642.