在DM6437中,关于EMAC的配置,需要配PLL和PINMUX。在C6455中好像没看到有相应的寄存器需要配置啊。C6455的EMAC使用是不需要配PLL和PINMUX吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在DM6437中,关于EMAC的配置,需要配PLL和PINMUX。在C6455中好像没看到有相应的寄存器需要配置啊。C6455的EMAC使用是不需要配PLL和PINMUX吗?
DSK6455的软件包里我没有看到这个配置啊.文档里也没看到关于PINMUX的软件寄存器配置。PLL中有关于EMAC的时钟配置吗?在哪个文档里有说?
6455 PLL USER'S GUIDE里貌似没有看到。
请参考6455 datasheet SPRS276M 7.8节 “PLL2 and PLL2 Controller”
我用的板子上,C6455的EMAC没有接PHY,直接连接的以太网交换芯片,该芯片自带有PHY,而且以太网交换芯片是通过其他芯片进行配置的。这种状况下,DSP的EMAC这边还需要单独配置PHY吗?