This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BBBlack开发板基于SD卡启动问题



如题:目前已经按照文献要求修改了DDR3的配置(参考帖子:www.deyisupport.com/.../73955.aspx),重新编译了bootloader代码(目录为AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\beaglebone\bootloader);采用的app为GPIOLED的程序(目录为AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\beaglebone\gpio);

操作步骤:

1)修改了DDR3的配置;

2)重新编译bootloader的工程,并在中生成了boot.ti.bin文件,目录为:                              AM335X_StarterWare_02_00_01_01\binary\armv7a\cgt_ccs\am335x\beaglebone\bootloader\Release_MMCSD,并将此文件重命名为:MLO文件;

3)重新编译gpio的工程,并生成gpioLEDBlink_ti.bin文件,目录为:

AM335X_StarterWare_02_00_01_01\binary\armv7a\cgt_ccs\am335x\beaglebone\gpio\Release,并将此文件重命名为:app文件;

4)初始化一块8GB的SD卡,并格式化为FAT格式,并存入之前的MLO和app文件;

5)插入SD卡,长按BOOT键,按住同时插入电源;

目前实验没有得到结果,有几个问题想询问:

1)编译bootloader代码需要设置启动模式为SD卡启动具体怎么操作,是不是如下图所示:

2)照理说bootloader加载image文件到SRAM,串口会打印字符,目前串口没有成功打印,请问这个串口是否为BBBlack中的J1口;

3)之前得到回复,需要校验PIN_MUX中的引脚寄存器,具体应该怎么操作,请详细告知。