This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6678CMD文件内地址分配的问题



工程师,您好!我在进行C6678开发的时候,在编写CMD文件时遇到一些疑问想向您确认一下,目前我们拟采用单核也就是core0进行开发,也不打算用SL2这段共享内存,在与FPGA通信时,FPGA端通过SRIO写入的数据放在DDR3_SRIO_fpga_0和 DDR3_SRIO_fpga_1这两段,同时DSP这边生成的数据存在DDR3_SRIO_DATA_1和DDR3_SRIO_DATA_2这两段,另外还有一些全局的比较大的数组,我直接定义在这些地址的后面DDR3_DATA,请问这样合理吗?

另外,想问一下,在编写cmd文件的时候还有什么需要注意的问题吗?

-heap  0x800
-stack 0x1000

MEMORY
{
 /* Local L2, 0.5~1MB*/
 BOOT_CORE1: o = 0x11800000,   l = 0x000000C0

 //VECTORS:   o = 0x10800400  l = 0x00000400
 //LL2_RW_DATA:  o = 0x10800800  l = 0x0002F800
 //VECTORS:   o = 0x10800000  l = 0x00000400
 //LL2_RW_DATA:  o = 0x10800400  l = 0x0002FC00

 //VECTORS:   o = 0x00800000  l = 0x00000400
 //LL2_RW_DATA:  o = 0x10800400  l = 0x0002FC00
 LL2_RW_DATA:  o = 0x11800400  l = 0x0002FC00

 //VECTORS:   o = 0x10810000  l = 0x00000400
 //LL2_RW_DATA:  o = 0x10810400  l = 0x0001FC00

 
 /* External DDR3, upto 2GB per core */
 DDR_fifo:  o = 0x80000000  l = 0x01000000   /*set memory protection attribitue as execution only*/
 DDR3_R_DATA:  o = 0x81000000  l = 0x01000000   /*set memory protection attribitue as read only*/
 DDR3_RW_DATA:  o = 0x82000000  l = 0x06000000   /*set memory protection attribitue as read/write*/

 DDR3_SRIO_DATA_1: o = 0x90000000  l = 0x00001F40   /*ToFPGA,8000字节*/
 DDR3_SRIO_DATA_2: o = 0x90001F40  l = 0x00001F40   /*ToFPGA,8000字节*/

 DDR3_SRIO_fpga_0: o = 0x90832000  l = 0x00001F40//FromFPGA,
 DDR3_SRIO_fpga_1: o = 0x90833F40  l = 0x00001F40//FromFPGA,透传过来的数据

DDR3_DATA: o = 0x90835E80  l = 0x00001F40//存储本地全局数据
 //DDR3_SRIO_fpga_1: o = 0x90832000  l = 0x00041000//FromFPGA可做数据读写操作的DDR空间

 //DDR_fifo:    o = 0x90000000  l = 0x00001000//fifo

}

SECTIONS
{
 //vecs        >    VECTORS

 .text           >    LL2_RW_DATA
 .cinit          >    LL2_RW_DATA
 .const          >    LL2_RW_DATA
 .switch         >    LL2_RW_DATA
 //.DDRText{MulticoreBoot.obj(.text)} > LL2_RW_DATA

 .stack          >    LL2_RW_DATA
 GROUP
 {
  .neardata
  .rodata
  .bss
 }   >    LL2_RW_DATA
 .far            >    LL2_RW_DATA
 .fardata        >    LL2_RW_DATA
 .cio            >    LL2_RW_DATA
 .sysmem         >    LL2_RW_DATA

 QMSS_Data.linkingRAM1   >  LL2_RW_DATA
 QMSS_Data.Descriptor_SL2  >  LL2_RW_DATA
 PacketData.buffer_SL2   >  LL2_RW_DATA
 PacketData.buffer_SL2   >  LL2_RW_DATA

 QMSS_Data.Descriptor_LL2  >  LL2_RW_DATA
 PacketData.buffer_LL2   >  LL2_RW_DATA
 PacketData.buffer_LL2   >  LL2_RW_DATA
 QMSS_Data.Descriptor_DDR  >  LL2_RW_DATA
 PacketData.buffer_DDR    > LL2_RW_DATA

 //Verify_addr.buffer > LL2_verify_addr
 //Verify_bytelen.buffer > LL2_verify_bytelen
 //CORE1.buffer > DDR3_SRIO_DATA_0
 //CORE1.buffer > CORE1_L2_put


 .myboot
     {
        *.*<boot.obj>(.text)

     } > BOOT_CORE1

}