DVRRDK_04.00.00.03_HDV8168 编码能支持H264/SVC格式,那么解码link支持SVC格式的解码吗 ?相关参数有哪些?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DVRRDK_04.00.00.03_HDV8168 编码能支持H264/SVC格式,那么解码link支持SVC格式的解码吗 ?相关参数有哪些?
Zhou Jarman,
请问你是解码DM8168的h264enc编码出来的SVC-T的码流么?还是解码其他设备编码出来的SVC码流?
Chris Meng
你好!
1.我目前流程是这样的,首先将一个AVC编码的文件(网络上下载)通过Declink解码之后 然后在EncLink指定SVC编码之后保存本地,查看码流会增加多个NALU单元(00 00 00 01 2E 80 80 07 20)单元内容如括号内,这样编码出来的码流是SVC-T的标准格式吗 ?
2.接下来我想将编码出来的SVC-T的264文件通过DecLink之后Display,可以实现吗?
Zhou Jarman,
如果只是解码DM81xx编码的SVC-T,建议你参考下面的文档,和DM81xx是类似的。
http://processors.wiki.ti.com/index.php/DM36x_temporal_SVC_application_note