This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642中断问题。求大神来carry!

初始化的时候中断寄存器的值是对的,但是程序一执行到建立视屏通路时寄存器的值就变了。

执行完上面的程序中断寄存器的值就变了,不能触发中断。

 EVMDM642_vDisParamsChan的代码如下:

VPORTDIS_Params EVMDM642_vDisParamsChan = {
VPORT_MODE_BT656_8BIT, /* dmode:3 */
VPORT_FLDOP_FRAME, /* fldOp:3 */

VPORT_SCALING_DISABLE, /* scale:1 */
// VPORT_SCALING_ENABLE, /* scale:1 */
VPORT_RESMPL_DISABLE, /* resmpl:1 */
VPORTDIS_DEFVAL_ENABLE,/* defValEn:1 */
VPORTDIS_BPK_10BIT_NORMAL, /*bpk10Bit:1 */

VPORTDIS_VCTL1_HSYNC, /* vctl1Config:2 */
VPORTDIS_VCTL2_VSYNC, /* vctl2Config:2 */
VPORTDIS_VCTL3_FLD, /* vctl3Config:1 */
VPORTDIS_EXC_DISABLE, /* extCtl:3 */

864, /* frmHSize */
625, /* frmVSize */

0, /* imgHOffsetFld1 */
0, /* imgVOffsetFld1 */
LINE_SZ, /* imgHSizeFld1 */
NUM_LINES, /* imgVSizeFld1 */

0, /* imgHOffsetFld2 */
0, /* imgVOffsetFld2 */
LINE_SZ, /* imgHSizeFld2 */
NUM_LINES, /* imgVSizeFld2 */

720, /* hBlnkStart */
862, /* hBlnkStop */

720, /* vBlnkXStartFld1 */
624, /* vBlnkYStartFld1 */
720, /* vBlnkXStopFld1 */
23, /* vBlnkYStopFld1 */

360, /* vBlnkXStartFld2 */
311, /* vBlnkYStartFld2 */
360, /* vBlnkXStopFld2 */
336, /* vBlnkYStopFld2 */

720, /* xStartFld1 */
1, /* yStartFld1 */

360, /* xStartFld2 */
313, /* yStartFld2 */

752, /* hSyncStart */
782, /* hSyncStop */

752, /* vSyncXStartFld1 */
1, /* vSyncYStartFld1 */
752, /* vSyncXStopFld1 */
3, /* vSyncYStopFld1 */

320, /* vSyncXStartFld2 */
313, /* vSyncYStartFld2 */
320, /* vSyncXStopFld2 */
316, /* vSyncYStopFld2 */

16, /* yClipLow */
235, /* yClipHigh */

16, /* cClipLow */
240, /* cClipHigh */
// 0, /* yClipLow */
// 255, /* yClipHigh */

// 0, /* cClipLow */
// 255, /* cClipHigh */

0x00,
0x80,
0x80,


VPORTDIS_RGBX_DISABLE, /* RGB extract disable */
0, /* incPix, for raw mode only */
(LINE_SZ>>3), /*thrld */

3, /*numFrmBufs*/
128, /*alignment */
VPORT_FLDS_MERGED, /*mergeFlds */
// VPORT_FLDS_SEPARATED, /*mergeFlds */
NULL, /*segId */
EDMA_OPT_PRI_HIGH, /*edmaPri */
10 /* irqId */
};