我现在有两块板子,其中一块为贵公司的LCDKOMAPL138开发板,并使用拓展口中的SPI0口与外部设备通信。另一块为参考此开发板电路设计的自己做的板子,而我们的板子使用的是SPI1口与外部设备通信。
现在分别在两块板子上跑程序,其中一部分是写SPI口的SPIPC4和SPIPC5寄存器来控制高低电平,发现相似的程序(主频300MHZ。程序中开发板使用SPI0基地址,自己做的板子使用SPI1基地址。PSC已唤醒,但PLL都未设置使用默认值)在两块板子上写SPIPC4和SPIPC5这两个寄存器的所用时间相差很大,差了十来倍的样子,所以我想知道写SPI口的寄存器所用时间与什么相关?是由于SPI0和SPI1差异导致的吗?