This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用XDS560v2仿真器连接6678DSP与PC 过程中,连接不上,同时test connection后显示如下结果是什么原因,该如何解决?急~

This error is generted by TI's USCIF driver or utilities.

The value is '-181'(0xffffff4b).

The title is 'SC-ERR_CTL_NO_TRG_CLOCK'.

The explanation is:

The controller has detected a dead JTAG clock.

The user must turn-on or connect the JTAG clock for the target.

[End: Wintcch Digital XDS 560v2 STM USB Emulator_0]

  • This error is shown when the JTAG debug probe does not receive a clock signal on the RTCK pin. It can have many reasons:

    • The speed of TCLK is configured for a rate too high for the board and device
    • The type of TCLK is configured for either fixed or adaptive but is unsupported by the device
    • The board PCB or device does not tie the TCK pin to the RTCK pin

    详情请参阅如下链接

    http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems?keyMatch=dead JTAG clock.&tisearch=Search-EN