This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 使用NandWriter的CCS工程烧写程序,配置完DDR2后,无法进入syncreset模式。

现在使用官方的NandWriter烧写程序,

发现配置完成DDR2,进行syncreset时,程序卡在device.c文件的

DEVICE_LPSCTransition(PSCNUM1, LPSC_EMIFB, PD0, PSC_SYNCRESET);这句话处,

进这个函数里面观察,发现前面虽然设置成syncreset,却根本无法切换到syncreset模式(一直在等待完成),也即只能一直停留在

// Wait for transition to complete

while ( (PSC->PTSTAT) & (0x00000001 << domain) );

请问:

1、DDR设置完成后,到底需不需要对这个DDR2模块进行syncreset?

2、如果需要syncreset,那么我这个问题可能出在什么地方?