This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678BootLoader的错误

我在6678开发板上使用SPI Nor Flash引导程序,参考例程是:www.deyisupport.com/.../8065.aspx。

在烧写工程使用的是:C:\ti\mcsdk_2_01_02_06\tools\writer\nor\evmc6678l

在烧写镜像文件时,点击“RUN”按钮后,出现了错误:

Can't find a source file at "/tmp/TI_MKLIBr78rCW/SRC/exit.c"
Locate the file or edit the source lookup path to include its location.

不知是什么原因?请大家解答一下,谢谢!

  • exit.c 文件没有找到,可能是路径不对,也可能是根本没有这个文件,不过这个应该不影响您烧写结果的

  • @Thomas Yang1

    你好,上面的提示估计不是错误的本质。

    把spirom_le.dat镜像文件load进入DDR3的0x8000 0000位置后,点击“RUN”按钮进行烧写,在console出现:

    [C66xx_0] NOR Writer Utility Version 01.00.00.03

    Error in parsing nor_writer_input.txt input file

    另外,弹出的对话框abort() at /tmp/TI_MKLIBr78rCW/SRC/exit.c:109 0x86f300

    Can't find a source file at "/tmp/TI_MKLIBr78rCW/SRC/exit.c"

    Locate the file or edit the source lookup path to include its location.


    就是烧写不成功,请问是什么原因呢?


    另外,看到很多例程都需要I2C的EEPROM里的程序作为引导,不知道这个是不是必须的?