专家你好,我用APPRO IPNC V2.6的开发包接入一个SONY的一体机机芯,在H2641080P单码流时,运行得很好。当我用双码流 1080P H264 + QVGA H264时,视频就会很卡,查看CPU使用率时,发现wis-streamer比平常占用了更多的CPU,估计是这个程序把CPU吃掉了,但是我用9p031这个SENSOR时,wis-streamer运行是正常的,所以 我想与wis-streamer无关。请问专家,是哪里出了问题呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问我能向您学习一下Appro方案的设计么?我是在校大学生,学习使用DM368 EVM的IPNC开发,现在已经安装了DVSDK4.02.00.06,环境也搭好了,但是在按照Avserver_UserGuider_Ipnc里的开发步骤执行make exe时总是会出现各种错误(因为我的ipnc_app、ipnc_capture是0.7.0版本的,lsp压缩包还是网上另下载的),我想问下:
1、dm368用4.02.00.06的dvsdk应该用哪个版本的Appro方案??
2.您能把Appro2.6的压缩包传我一份么??252360872@qq.com
请大神指导下,鄙人非常感激。。。
请问下,我最近也在搞这个,版本也是2.6,SONy一体机是EH6300,但是不知道为什么我的总是没数据过来,好像是没中断过来,兄台有遇到这种状况吗?我接过GV7601也是YUV422 16bit 的格式可以,但是为什么接一体机不行???