Other Parts Discussed in Thread: AM5728
请问AM5728是否支持同时两路视频输出?
如果支持,每路支持的视屏格式和要求是多大的?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Display Subsystem (DSS) provides the logic to display a video frame from the system memory frame
buffer on a liquid-crystal display (LCD) panel or TV set.
The display subsystem can display different pictures simultaneously by using three LCD outputs (LCD1,
LCD2, and LCD3), in addition to a TV output.
All three LCD outputs are available on three parallel interfaces (DPI1, DPI2, and DPI3), providing support
for MIPI DPI 2.0, or BT-656 or BT-1120.
The TV output is available on one of the following interfaces
• High-Definition Multimedia Interface (HDMI)
• DPI1 parallel interface
The modules integrated in the display subsystem are:
• Display controller (DISPC):
– One direct memory access (DMA) engine
– One graphics pipeline (GFX), three video (VID) pipelines, and one write-back (WB) pipeline
– Three LCD outputs and one TV output, each with a dedicated overlay manager
• HDMI protocol engine:
– HDMI 1.4a support up to 1080p@60Hz (including 3D frame-packing support)
– 36-bit RGB color
– HDCP 1.4 key protection
– Deep color mode support (10-bit/12-bit for 148.5-MHz pixel clock)
最多四路,具体可以看TRM