This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK编译问题



最近在学习NDK的使用方法,看到Rebuilding NDK Libraries部分,根据手册指示,我在TI官网上看到有Rebuilding the NDK Core和Rebuilding The NDK Core Using Gmake 两部分内容,文中说Rebuilding the NDK Core适用于NDK 2.20.(These instructions apply to NDK 2.20. To rebuild libraries for NDK 2.21 using Gmake, please refer to processors.wiki.ti.com/.../Rebuilding_The_NDK_Core_Using_Gmake),而Rebuilding The NDK Core Using Gmake适用于2.21 和更高版本(These instructions apply to NDK version 2.21 (and higher) only. For instructions on how to (re)build NDK 2.20x, please refer to processors.wiki.ti.com/.../Rebuilding_the_NDK_Core)。我想问一下使用Rebuilding the NDK Core提供的方法能编译2.21 版本吗?因为本人对Gmake这种方式不太熟悉,而我使用的又是2.21 版本。