This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【Bootloader】6678 SPI NOR FLASH加载问题

您好:

请教的问题如下:6678的评估板上把DSP的SPI1接到了FPGA上(从FPGA读取和配置一些状态),6678从NOR FLASH加载或者从NAND flash加载(利用EEPROM的二次加载)时需要用到这个SPI1从FPGA获取配置信息吗?目前,我们自己设计的板子没有把DSP的SPI1接到FPGA上,不管是NOR还是NAND都加载不起来。

期待您的回复~

  • 6678 RBL支持SPI可以直接接nand flash进行flash加载,可以不接FPGA,论坛中有spi flash加载的例程参考。

  • 您是说如果采用SPI模式一次加载的话不需要FPGA,也不需要EEPROM吗?

    那采用NOR FLash二次加载的话,就必须将DSP的SPI1接到FPGA,在boot时通过SPI1口从FPGA读取配置信息,是这样吗?我的理解是二次加载DSP从EEPROM获取parameter table等信息,为什么还需要从FPGA读取配置信息呢

    期待您的回复,谢谢~