This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6670 nimu_eth_evmc6670l工程导入问题



  我需要修改nimu_eth.c函数里的程序,现在导入该工程的时候发现工程目录下nimu_eth_evmc6670l 打不开,然后程序编译的时候就失败了。

编译结果为:
 *** Build Finished ****

**** Build of configuration Debug for project nimu_eth_evmc6670l ****

"D:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 
'Building file: ../nimu_lib.cfg'
'Invoking: XDCtools'
"D:/ti/xdctools_3_23_04_60" --xdcpath="D:/ti/ndk_2_21_01_38/packages;D:/ti/bios_6_33_06_50/packages;D:/tik_C6670_1_1_2_5/packages;D:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.platforms.evm6670 -r whole_program -c "D:/ti/C6000 Code Generation Tools 7.4.2" "../nimu_lib.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring nimu_lib.pe66 from package/cfg/nimu_lib_pe66.cfg ...
cle66 package/cfg/nimu_lib_pe66.c ...
Fatal error: could not open source file "Code"
1 fatal error detected in the compilation of "Code".
Compilation terminated.

>> Compilation failure
gmake.exe: *** [package/cfg/nimu_lib_pe66.oe66] Error 1
js: "D:/ti/xdctools_3_23_04_60/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: *** [configPkg/compiler.opt] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

我不知道哪儿出错了,恳请大家帮忙一下,该怎么解决。