This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168芯片1.0-AVS电压控制电路疑问&以及SmartReflex的工作机制

1、1.0-AVS电压1.0V固定供电是否可以?(现有设计的十几块板子都未发现问题):

2、对芯片的SmartReflex功能,有几点疑惑希望能够得到解决:

1)参考电路如下

2)参考8168的EVM板进行设计,电源芯片换成了TPS40192DRCR,MOS管也进行物料更改,想知道该电路是否满足AVS电路要求?

4)文档中AVS电压调节范围“”0.8V-1.05V“”,那我设计的电阻网络是否就可以按照这个电压范围进行设计?16个电压等级,固有电压步进按照15mV进行设计?

5)硬件上是否只要有上述电路就可以满足SmartReflex工作要求,是否需要添加电流监测电路?(手头上的板子没有设计这部分电路)

6)如果硬件都能满足,那是否就只需要软件方面配合就能实现功能?且实现功能方式是怎样?主要是8168芯片内部通过监测电压,温度以及系统工作进程,进行AVS电压调节?

7)上电时,AVS默认电压要1.0V,之后芯片在自动调节?使用MOS管进行AVS在电调节电压时,电源电压是否会有毛刺等影响芯片工作?且在调节电压期间,芯片是否可能工作异常?

希望得到TI工程师们的支持,谢谢!

  • 你好,

    不建议在AVS电压管脚上使用固定电压,有可能导致系统不稳定。

    关于AVS的信息,你是否有参考过以下链接的内容?

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_AVS_FAQ

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_PM_AVS_Driver_User_Guide