This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 内核启动卡死问题(Uncompressing Linux... done, booting the kernel.)



我使用DM8168板子 开机启动时 偶尔会出现卡死情况 不只是什么原因,正在查找,请问有没有建议


U-Boot 2010.06 (Jan 17 2017 - 18:46:34)

TI8168-GP rev 2.1

HDVICP clk : 600MHz
L3 Fast clk : 560MHz
HDVPSS clk : 280MHz
Ducati M3 clk : 280MHz
DSP clk : 1000MHz
ARM clk : 987MHz
DDR clk : 675MHz

I2C: ready
DRAM: 2 GiB
NAND: HW ECC BCH8 Selected
512 MiB
MMC: OMAP SD/MMC: 0
zigsun:8003
LEVEL:micron
EMIF0_PBBPR:0x30

Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:84:7e:40:ef:fc:2
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 0

Loading from NAND 512MiB 3,3V 8-bit, offset 0x580000
Image Name: Linux-2.6.37-2.0.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2981404 Bytes = 2.8 MiB
Load Address: c0008000
Entry Point: c0008000
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37-2.0.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2981404 Bytes = 2.8 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

[kernel] Uncompressing Linux... done, booting the kernel.

  • Luo Yu,

    会不会是DDR稳定性问题?如果降低DDR频率是否有改善?

    请问你们的DDR布线是否100%按照数据手册的要求来做。DDR的时序参数是否有根据你们使用的DDR芯片调整过?DDR SW levelign是否有做过?