This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求一个C6748的UPP操作的demo



我在 pspdrivers_01_30_01 文件夹下找到了几个upp的demo,不过它们都是基于dsp/bios操作系统的,符合IOM的驱动模型,我感觉这样操作upp是不是会有点麻

烦呀,在C6748_StarterWare_1_20_04_01 下面有很多裸机驱动和demo,就是没有upp的裸机demo。

问题:

1、有没有upp的裸机demo,能不能发个链接啊?

2、如果采用dsp/bios  IOM驱动模型的upp,为了统一性,那么其他模块(比如gpio、spi等),是不是也最好采用dsp/bios 下的写法来操作?

3、官方给的IOM驱动模型的upp  demo是基于dsp/bios5.41的,而现在我都已经用上CCSV 6版本软件了,相应的操作系统也都更新了,现在都是sys/bios了,比

如我用一个sys/bios 6.42,那么原来这个dsp/bios5.41的IOM upp驱动,是不是也要做些更改?

4、根据我的观察,dsp/bios5.41到sys/bios转变时,除了SIO相关函数向GIO函数调整外,调用的底层的文件upp.c也有少许变化(主要是命名的变化,可能还有极

少的内容变化),经过努力,这个upp模块终于成功编译通过了。为保持统一性,如果其他模块也想在sys/bios下操作,也需要注意一下dsp/bios5.41到sys/bios时

可能的驱动变化吧?

5、然后,我又试着写了一个gpio的操作,不像操作upp时的变化,这次驱动好像没啥需要变化的,但因为没有操作其他模块,也不知到它们的工作量大不大。这种

情况,能不能给个建议,究竟用裸机操作好些,还是带着sys/bios好些呢?