Other Parts Discussed in Thread: SYSBIOS
您好,
请问一下你们有关于AM335x平台上移植uCOS方面的参考吗,或者有什么经验吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是对于实时性的处理,我看过ti官方的sysbios系统,但是关于这方面的demo比较少,我也试着去使用了一下,不知道为何仿真就出错,这是我的代码:
Int main()
{
Task_Handle task;
Error_Block eb;
Task_Params taskParams;
/* Enabling functional clocks for GPIO1 instance. */
GPIO1ModuleClkConfig();
/* Selecting GPIO1[23] pin for use. */
GPIO1Pin23PinMuxSetup();
UARTSetup();
/* Enabling the GPIO module. */
GPIOModuleEnable(GPIO_INSTANCE_ADDRESS);
/* Resetting the GPIO module. */
GPIOModuleReset(GPIO_INSTANCE_ADDRESS);
/* Setting the GPIO pin as an output pin. */
GPIODirModeSet(GPIO_INSTANCE_ADDRESS,
GPIO_INSTANCE_PIN_NUMBER,
GPIO_DIR_OUTPUT);
UARTPuts("Enter StarterWare Application...\r\n\n", -1);
System_printf("enter main()\n");
Task_Params_init(&taskParams);
taskParams.stackSize = 20480;
taskParams.priority = 1;
Error_init(&eb);
task = Task_create(taskFxn, &taskParams, &eb);
taskParams.priority = 2;
task = Task_create(taskFx1, &taskParams, &eb);
taskParams.priority = 3;
task = Task_create(taskFx2, &taskParams, &eb);
if (task == NULL) {
System_printf("Task_create() failed!\n");
BIOS_exit(0);
}
BIOS_start(); /* does not return */
return(0);
}
仿真后的结果:
[CortxA8] 0x44e000ac R8 = 0x4030d028
R1 = 0x00000000 R9 = 0x4030d008
R2 = 0x00000064 R10 = 0x4030d484
R3 = 0xfffffffd R11 = 0x00029940
R4 = 0x00000000 R12 = 0xffffffff
R5 = 0x00000200 SP(R13) = 0x800095e0
R6 = 0x48060000 LR(R14) = 0x800111dc
R7 = 0x00000020 PC(R15) = 0x800095e0
PSR = 0x48060000
DFSR = 0x00000005 IFSR = 0x00000000
DFAR = 0x44e000ac IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x800095e0, lr = 0x800111dc.
xdc.runtime.Error.raise: terminating execution
然后就跳入
static void loader_exit(void)
{
#if defined(EMBED_CIO_BP)
__asm(" .global C$$EXITE");
#if defined(__32bis__)
__asm("C$$EXITE:.word 0xDEFED0FE");
#else
__asm(" .align 4");
#if defined(__big_endian__)
__asm("C$$EXITE:.half 0xDEFE");
#else
__asm("C$$EXITE:.half 0xD0FE");
#endif /* __big_endian__ */
#endif /* __32bis__ */
#else /* !EMBED_CIO_BP */
__asm(" .global C$$EXIT");
__asm("C$$EXIT: nop");
#endif
}
请教一下这是什么原因呢?