This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

edma传输参数设置问题

edma传输中,采用AB模式传输,设置SRCBIDX参数时,发现写为0x8000时,只传输一个A大小的数据,余下(B-1)次没有传输,do_while循环也可跳过,但是改为0x7ff0,或者0x6000,都可以传输正确,而且发现写为0x8100便也不正确,查edma文献里说BIDX上线是65535(0xffff),嗯,请问会是什么原因呢?谢谢   myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_EN, \

                                            CSL_EDMA3_TCCH_DIS, \

                                            CSL_EDMA3_ITCINT_DIS, \

                                            CSL_EDMA3_TCINT_EN, \

                                            0, CSL_EDMA3_TCC_NORMAL,\

                                            CSL_EDMA3_FIFOWIDTH_NONE, \

                                            CSL_EDMA3_STATIC_DIS, \

                                            CSL_EDMA3_SYNC_AB, \

                                            CSL_EDMA3_ADDRMODE_INCR, \

                                            CSL_EDMA3_ADDRMODE_INCR );

   myParamSetup.srcAddr    = (Uint32)ptr_srcBuff;

   myParamSetup.aCntbCnt   = CSL_EDMA3_CNT_MAKE(8,128);                            //AB模式传输

   myParamSetup.dstAddr    = (Uint32)dstBuff;                                      //如果是A模式传输,则B,C索引值没有用到

   myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(0x8010,8);                          //如果是AB模式传输,则C索引值没有用到

   myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);

   myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);

   myParamSetup.cCnt = 1;