This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl138 修改CPU频率参数



Hello all,

           想确认一下如果想把OMAPl138 的主频从300 MHz调到 456 MHz,需要把 OMAPL138_LCDK.gel 文件里的 Core_300MHz_mDDR_150MHz()改成Core_456MHz_mDDR_150MHz(), 以及soc_OMAPL138.h 里的#define SOC_SYSCLK_1_FREQ                   (300000000) 改成456000000, 除了这些还有什么需要update吗?

          谢谢大家啦,新春快乐呀

Dee

    Core_300MHz_mDDR_150MHz();