This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师您好,我在调试C6678的过程中,从DDR的一块地址向FPGA写数据,采用的是流写方式,长度是512个字节,但是在FPGA端读出来的数据发现是乱序的,而且在写的过程中还会出现SRIO的port_ok位为0的情况,想请问一下可能是什么原因?之前测的FPGA端到DSP这端写数据是正常的。
麻烦工程师能够解答一下!
有如下几项建议测试一下:
1 内存放到L2中测试下呢
2 如果SRIO PORT_OK有时为非0,证明SRIO LINK还不稳定,建议先把链路调稳定再说
3 检查下SRIO错误状态寄存器看看