This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138上用EDMA访问SPI的例程

分享一个在OMAPL138上用EDMA访问SPI的例程。

SPI_EDMA_ARM_L138.zip
  • 为啥下载不了?

  • 下载不了了,能不能给我邮箱发一份啊,我的邮箱是zjrayw168@163.com,非常感谢!!!!

  • 能否共享一下,邮箱 hanjia0604@126.com,,此外想咨询一下用CCS3.3 写ARM端的中断怎么写?尤其是asm文件,谢谢

  • 更新了。现在可以下载了。你的第二个问题另起一个贴子吧。

  • 看楼主的名字,好像是TI深圳办事处的?

     

  • 是的,你在做什么项目,在什么公司,我们可以用邮箱联系。

  • 我用楼主的ASM文件可以实现中断,但是又出现其他问题,我的串口函数只能收,不能发,用我原来的asm文件,串口收发是没有问题的。我用的是UART0

    极度郁闷,希望高手提点。qq147699355 邮箱 hanjia0604@126.com

    我的asm文件如下;

    ;******************************************************************************
    ;* BOOT  v4.6.4                                                               *
    ;* Copyright (c) 1996-2010 Texas Instruments Incorporated                     *
    ;******************************************************************************

    ;****************************************************************************
    ;* BOOT.ASM
    ;*
    ;* THIS IS THE INITAL BOOT ROUTINE FOR TMS470 C++ PROGRAMS.
    ;* IT MUST BE LINKED AND LOADED WITH ALL C++ PROGRAMS.
    ;*
    ;* THIS MODULE PERFORMS THE FOLLOWING ACTIONS:
    ;*   1) ALLOCATES THE STACK AND INITIALIZES THE STACK POINTER
    ;*   2) CALLS AUTO-INITIALIZATION ROUTINE
    ;*   3) CALLS THE FUNCTION MAIN TO START THE C++ PROGRAM
    ;*   4) CALLS THE STANDARD EXIT ROUTINE
    ;*
    ;* THIS MODULE DEFINES THE FOLLOWING GLOBAL SYMBOLS:
    ;*   1) __stack     STACK MEMORY AREA
    ;*   2) _c_int00    BOOT ROUTINE
    ;*
    ;****************************************************************************
       .if  __TI_TMS470_V7M3__
     .thumbfunc _c_int00
       .else
     .armfunc _c_int00
       .endif

    ;****************************************************************************
    ; Accomodate different lowerd names in different ABIs
    ;****************************************************************************
       .if   __TI_EABI_ASSEMBLER
            .asg _args_main,   ARGS_MAIN_RTN
            .asg exit,         EXIT_RTN
            .asg    main_func_sp, MAIN_FUNC_SP
       .elseif __TI_ARM9ABI_ASSEMBLER | .TMS470_32BIS
            .asg __args_main,   ARGS_MAIN_RTN
            .asg _exit,         EXIT_RTN
            .asg    _main_func_sp, MAIN_FUNC_SP
       .else
            .asg $_args_main,   ARGS_MAIN_RTN
            .asg $exit,         EXIT_RTN
            .asg    _main_func_sp, MAIN_FUNC_SP
       .endif

       .if .TMS470_16BIS

    ;****************************************************************************
    ;*  16 BIT STATE BOOT ROUTINE                                               *
    ;****************************************************************************

       .if __TI_TMS470_V7M3__
     .state16
       .else
     .state32
       .endif

     .global __stack
    ;***************************************************************
    ;* DEFINE THE USER MODE STACK (DEFAULT SIZE IS 512)              
    ;***************************************************************
    __stack:.usect ".stack", 0, 4

     .global _c_int00

    ;***************************************************************
    ;* FUNCTION DEF: _c_int00                                     
    ;***************************************************************
    _c_int00: .asmfunc

     .if !__TI_TMS470_V7M3__
     .if __TI_NEON_SUPPORT__ | __TI_VFP_SUPPORT__
            ;*------------------------------------------------------
     ;* SETUP PRIVILEGED AND USER MODE ACCESS TO COPROCESSORS
     ;* 10 AND 11, REQUIRED TO ENABLE NEON/VFP     
     ;* COPROCESSOR ACCESS CONTROL REG
     ;* BITS [23:22] - CP11, [21:20] - CP10
     ;* SET TO 0b11 TO ENABLE USER AND PRIV MODE ACCESS
            ;*------------------------------------------------------
     MRC      p15,#0x0,r0,c1,c0,#2
            MOV      r3,#0xf00000
     ORR      r0,r0,r3
            MCR      p15,#0x0,r0,c1,c0,#2

            ;*------------------------------------------------------
     ; SET THE EN BIT, FPEXC[30] TO ENABLE NEON AND VFP
            ;*------------------------------------------------------
           MOV      r0,#0x40000000
            FMXR     FPEXC,r0
     .endif

     ;------------------------------------------------------
     ;* SET TO USER MODE
            ;*------------------------------------------------------
            MRS     r0, cpsr
            BIC     r0, r0, #0x1F  ; CLEAR MODES
            ORR     r0, r0, #0x10  ; SET USER MODE
            MSR     cpsr_cf, r0

            ;*------------------------------------------------------
     ;* CHANGE TO 16 BIT STATE
            ;*------------------------------------------------------
     ADD r0, pc, #1
     BX r0

     .state16
     .endif

     ;*------------------------------------------------------
            ;* INITIALIZE THE USER MODE STACK                     
            ;*------------------------------------------------------
     LDR     r0, c_stack
     MOV sp, r0
            LDR     r0, c_STACK_SIZE
     ADD sp, r0

     ;*-----------------------------------------------------
     ;* ALIGN THE STACK TO 64-BITS IF EABI.
     ;*-----------------------------------------------------
     .if __TI_EABI_ASSEMBLER
     MOV r7, sp
     MOV r0, #0x07
     BIC     r7, r0         ; Clear upper 3 bits for 64-bit alignment.
     MOV sp, r7
     .endif

     ;*-----------------------------------------------------
     ;* SAVE CURRENT STACK POINTER FOR SDP ANALYSIS
     ;*-----------------------------------------------------
     LDR r0, c_mf_sp
     MOV r7, sp
     STR r7, [r0]

            ;*------------------------------------------------------
            ;* Perform all the required initilizations:
            ;*   - Process BINIT Table
            ;*   - Perform C auto initialization
            ;*   - Call global constructors
            ;*------------------------------------------------------
            BL      __TI_auto_init

            ;*------------------------------------------------------
     ;* CALL APPLICATION                                    
            ;*------------------------------------------------------
            BL      ARGS_MAIN_RTN

            ;*------------------------------------------------------
     ;* IF APPLICATION DIDN'T CALL EXIT, CALL EXIT(1)
            ;*------------------------------------------------------
            MOV     r0, #1
            BL      EXIT_RTN

            ;*------------------------------------------------------
     ;* DONE, LOOP FOREVER
            ;*------------------------------------------------------
    L1:     B L1
     .endasmfunc

       .else           ; !.TMS470_16BIS

    ;****************************************************************************
    ;*  32 BIT STATE BOOT ROUTINE                                               *
    ;****************************************************************************

     .global __stack
    ;***************************************************************
    ;* DEFINE THE USER MODE STACK (DEFAULT SIZE IS 512)           
    ;***************************************************************
    __stack:.usect ".stack", 0, 4

     .global _c_int00
    ;***************************************************************
    ;* FUNCTION DEF: _c_int00                                     
    ;***************************************************************
    _c_int00: .asmfunc

     .if __TI_NEON_SUPPORT__ | __TI_VFP_SUPPORT__
            ;*------------------------------------------------------
     ;* SETUP PRIVILEGED AND USER MODE ACCESS TO COPROCESSORS
     ;* 10 AND 11, REQUIRED TO ENABLE NEON/VFP     
     ;* COPROCESSOR ACCESS CONTROL REG
     ;* BITS [23:22] - CP11, [21:20] - CP10
     ;* SET TO 0b11 TO ENABLE USER AND PRIV MODE ACCESS
            ;*------------------------------------------------------
     MRC      p15,#0x0,r0,c1,c0,#2
            MOV      r3,#0xf00000
     ORR      r0,r0,r3
            MCR      p15,#0x0,r0,c1,c0,#2

            ;*------------------------------------------------------
     ; SET THE EN BIT, FPEXC[30] TO ENABLE NEON AND VFP
            ;*------------------------------------------------------
           MOV      r0,#0x40000000
            FMXR     FPEXC,r0
     .endif

            ;*------------------------------------------------------
     ;* SET TO USER MODE
            ;*------------------------------------------------------
            MRS     r0, cpsr
            BIC     r0, r0, #0x1F  ; CLEAR MODES
            ORR     r0, r0, #0x13  ; SET USER MODE
            MSR     cpsr_cf, r0

            ;*------------------------------------------------------
            ;* INITIALIZE THE USER MODE STACK                     
            ;*------------------------------------------------------
     LDR     sp, c_stack
            LDR     r0, c_STACK_SIZE
     ADD sp, sp, r0

     ;*-----------------------------------------------------
     ;* ALIGN THE STACK TO 64-BITS IF EABI.
     ;*-----------------------------------------------------
     .if __TI_EABI_ASSEMBLER
     BIC     sp, sp, #0x07  ; Clear upper 3 bits for 64-bit alignment.
     .endif

     ;*-----------------------------------------------------
     ;* SAVE CURRENT STACK POINTER FOR SDP ANALYSIS
     ;*-----------------------------------------------------
     LDR r0, c_mf_sp
     STR sp, [r0]
                   
            ;*------------------------------------------------------
            ;* Perform all the required initilizations:
            ;*   - Process BINIT Table
            ;*   - Perform C auto initialization
            ;*   - Call global constructors
            ;*------------------------------------------------------
            BL      __TI_auto_init

            ;*------------------------------------------------------
     ;* CALL APPLICATION                                    
            ;*------------------------------------------------------   
            BL      ARGS_MAIN_RTN

            ;*------------------------------------------------------
     ;* IF APPLICATION DIDN'T CALL EXIT, CALL EXIT(1)
            ;*------------------------------------------------------
            MOV     R0, #1
            BL      EXIT_RTN

            ;*------------------------------------------------------
     ;* DONE, LOOP FOREVER
            ;*------------------------------------------------------
    L1:     B L1
     .endasmfunc

       .endif    ; !.TMS470_16BIS

    ;***************************************************************
    ;* CONSTANTS USED BY THIS MODULE
    ;***************************************************************
    c_stack  .long    __stack
    c_STACK_SIZE   .long    __STACK_SIZE
    c_mf_sp         .long    MAIN_FUNC_SP

     .if __TI_EABI_ASSEMBLER
            .data
            .align 4
    _stkchk_called:
            .field          0,32
            .else
            .sect   ".cinit"
            .align  4
            .field          4,32
            .field          _stkchk_called+0,32
            .field          0,32

            .bss    _stkchk_called,4,4
            .symdepend ".cinit", ".bss"
            .symdepend ".cinit", ".text"
            .symdepend ".bss", ".text"
     .endif

    ;******************************************************
    ;* UNDEFINED REFERENCES                               *
    ;******************************************************
     .global _stkchk_called
     .global __STACK_SIZE
     .global ARGS_MAIN_RTN
     .global MAIN_FUNC_SP
     .global EXIT_RTN
        .global __TI_auto_init

     .end

  • Hai,Tony,您的邮箱多少呢?有些项目信息想和您交流一下。
  • 能否共享一个EDMA方式读取EMIFA数据的例程。不胜感激!

  • EDMA访问EMIFA需要通过其它手段来触发,如GPIO等,所以你需要参考另一个例程GPIO触发EDMA传输。

  • 单核的C6748使用EDMA3读SPI1 ,总是没有反应,请问也需要什么触发么

  • pinmux,psc配置对了没有。

  • 一直被一个问题困扰着,就是ARM核要用SPI的EDMA,DSP核要用mcasp的EDMA,但是这两个EDMA通道怒属于同一个edma控制器,但是手册上写着同一个edma控制器有4个EDMA3_0_CC0_INT[3:0],但是在库.h的中断向量表里面同一个EDMA控制器只有一个中断完成向量,两个核可以同时用中断的方式使用同一个EDMA通道控制器的不同通道吗?比如ARM用SPI EDMA中断方式,DSP用MCASP EDMA中断方式,如果可以的话怎么用?因为我在库文件里面只找到一个中断向量,但是芯片手册里面有4个中断向量。

  • #1. SPI与EDMA都属于CC0的事件。

    #2. CC0在AINTC上有中断号EDMA3_0_CC0_INT0,在DSP上有事件EDMA3_0_CC0_INT1。

    #3. 那么要同时用,则在ARM端通过EDMA的shadow region 0控制SPI的EDMA, 在DSP端通过shadow region 1 控制MCASP的EDMA就可以了。

    BWT,我没看到有4个shadow region的中断事件EDMA3_0_CC0_INT[3:0],只看到2个EDMA3_0_CC0_INT[1:0]

  • tony edma通道控制器错误处理只有一个中断向量,但是它在双核里面都对应一个中断号,双核里面可以同时注册同一个edma通道控制器错误处理中断嘛?
  • bingliang chen 说:
    edma通道控制器错误处理只有一个中断向量,但是它在双核里面都对应一个中断号,双核里面可以同时注册同一个edma通道控制器错误处理中断嘛?

    理论上是可以,因为中断事件的产生可以分发到两个中断控制器,两个中断控制器都会收到这个中断信号,如果两边都使能了,则都会进入中断服务程序,剩下的看你软件怎么处理了。

x 出现错误。请重试或与管理员联系。