This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148采集显示编码失败问题求助



各位大神,我使用TI DM8148 在编码时出现了问题,我的数据链路是cap---dup----sws---dis

                                                                                                                                      |---encode

采集的数据经过dup后分两路,一路进行显示dis.另一路经过encode编码,dis可以正常显示,但encode出现了问题,实在找不到问题所在,希望大神们给予指点。

说明:1)输入源为HDMI 1080p60 逐行模式。

以下为部分代码贴图与LOG信息

int main(int argc, char **argv) {
signal(SIGINT, sig_handle);

/* System init */
VSYS_PARAMS_S vsysParams;
Vsys_params_init(&vsysParams);
Vsys_init(&vsysParams);

/* Capture init */
VCAP_PARAMS_S vcapParams;
Vcap_params_init(&vcapParams);
Vcap_init(&vcapParams);

/* Encode init */
VENC_PARAMS_S vencParams;
Venc_params_init(&vencParams);
/* Enable B frame for primary channels - set parameters before venc_init */
int ch;
for (ch=0; ch < CH_NUM; ch++)
vencParams.encChannelParams[ch].dynamicParam.interFrameInterval =I_TO_P_FRAME_INTERVAL_FOR_PRIMARY_STREAMS;
Venc_init(&vencParams);

/* Display init */
VDIS_PARAMS_S vdisParams;
Vdis_params_init(&vdisParams);
vdisParams.deviceParams[VDIS_DEV_HDMI].resolution = VSYS_STD_1080P_60;
vdisParams.mosaicLayoutResolution[VDIS_DEV_HDMI] = vdisParams.deviceParams[VDIS_DEV_HDMI].resolution;
vdisParams.mosaicParams[VDIS_DEV_HDMI].userSetDefaultSWMLayout = TRUE;

Vdis_init(&vdisParams);

/* Configure display */
Vsys_configureDisplay();

/* Init the application specific module which will handle bitstream exchange */
bits_saver_create(CH_NUM, "h264");

void chain_cap_enc_dis_create()

{.......

MultiCh_detectBoard();

System_linkControl(
SYSTEM_LINK_ID_M3VPSS,
SYSTEM_M3VPSS_CMD_RESET_VIDEO_DEVICES,
NULL,
0,
TRUE
);

System_linkControl(
SYSTEM_LINK_ID_M3VIDEO,
SYSTEM_COMMON_CMD_SET_CH2IVAHD_MAP_TBL,
&systemVid_encDecIvaChMapTbl,
sizeof(SystemVideo_Ivahd2ChMap_Tbl),
TRUE
);

gVcapModuleContext.captureId = SYSTEM_LINK_ID_CAPTURE;
gVcapModuleContext.nsfId[0] = SYSTEM_LINK_ID_NSF_0;
gVencModuleContext.encId = SYSTEM_LINK_ID_VENC_0;

gVdisModuleContext.swMsId[0] = SYSTEM_LINK_ID_SW_MS_MULTI_INST_0;
gVdisModuleContext.displayId[0] = SYSTEM_LINK_ID_DISPLAY_0;
gVcapModuleContext.deiId[0] = SYSTEM_LINK_ID_DEI_0;


dupId[0] = SYSTEM_VPSS_LINK_ID_DUP_0;
dupId[1] = SYSTEM_VPSS_LINK_ID_DUP_1;

UInt32 ipcOutVpssId = SYSTEM_VPSS_LINK_ID_IPC_OUT_M3_0;
UInt32 ipcInVideoId = SYSTEM_VIDEO_LINK_ID_IPC_IN_M3_0;


gVencModuleContext.ipcBitsOutRTOSId = SYSTEM_VIDEO_LINK_ID_IPC_BITS_OUT_0;
gVencModuleContext.ipcBitsInHLOSId = SYSTEM_HOST_LINK_ID_IPC_BITS_IN_0;
gVdecModuleContext.ipcBitsOutHLOSId = SYSTEM_HOST_LINK_ID_IPC_BITS_OUT_0;
gVdecModuleContext.ipcBitsInRTOSId = SYSTEM_VIDEO_LINK_ID_IPC_BITS_IN_0;

/* capture link init */
CaptureLink_CreateParams_Init(&capturePrm);
capturePrm.numVipInst = 1;
capturePrm.outQueParams[0].nextLink = dupId[0];
capturePrm.tilerEnable = FALSE;
capturePrm.enableSdCrop = FALSE;
capturePrm.numBufsPerCh = 8;
capturePrm.maxBlindAreasPerCh = 4;

/* capture instance init */
CaptureLink_VipInstParams *prm_cap_inst = &capturePrm.vipInst[0];
prm_cap_inst->vipInstId = (SYSTEM_CAPTURE_INST_VIP0_PORTA + 0 ) % SYSTEM_CAPTURE_INST_MAX;
prm_cap_inst->videoDecoderId = DEVICE_VID_DEC_ADV7610_DRV;
prm_cap_inst->inDataFormat = SYSTEM_DF_YUV422P;
prm_cap_inst->standard = SYSTEM_STD_1080P_60;
prm_cap_inst->numOutput = 1;
prm_cap_inst->videoIfMode = DEVICE_CAPT_VIDEO_IF_MODE_16BIT;
prm_cap_inst->videoCaptureMode = DEVICE_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_EMBEDDED_SYNC;

/* capture out init */
CaptureLink_OutParams *prm_cap_out = &prm_cap_inst->outParams[0];
prm_cap_out->dataFormat = SYSTEM_DF_YUV420SP_UV;//SYSTEM_DF_YUV422I_YUYV;
prm_cap_out->scEnable = FALSE;
prm_cap_out->scOutWidth = 0;
prm_cap_out->scOutHeight = 0;
prm_cap_out->outQueId = 0;

EncLink_CreateParams_Init(&encPrm);
encPrm.numBufPerCh[0] = 4;
for (i = 0; i < NUM_CH; i++) {
#if 1

EncLink_ChCreateParams *pLinkChPrm = &encPrm.chCreateParams[i];
VENC_CHN_PARAMS_S *pChPrm = &gVencModuleContext.vencConfig.encChannelParams[i];

pLinkChPrm->format = IVIDEO_H264HP;
pLinkChPrm->profile = gVencModuleContext.vencConfig.h264Profile[i];
pLinkChPrm->dataLayout = VCODEC_FIELD_SEPARATED;
pLinkChPrm->fieldMergeEncodeEnable = FALSE;
pLinkChPrm->enableAnalyticinfo = pChPrm->enableAnalyticinfo;
pLinkChPrm->enableWaterMarking = pChPrm->enableWaterMarking;
pLinkChPrm->maxBitRate = pChPrm->maxBitRate;
pLinkChPrm->encodingPreset = pChPrm->encodingPreset;
pLinkChPrm->rateControlPreset = pChPrm->rcType;
pLinkChPrm->enableSVCExtensionFlag = pChPrm->enableSVCExtensionFlag;
pLinkChPrm->numTemporalLayer = pChPrm->numTemporalLayer;

EncLink_ChDynamicParams *pLinkDynPrm = &pLinkChPrm->defaultDynamicParams;
VENC_CHN_DYNAMIC_PARAM_S *pDynPrm = &pChPrm->dynamicParam;

pLinkDynPrm->intraFrameInterval = pDynPrm->intraFrameInterval;
pLinkDynPrm->targetBitRate = pDynPrm->targetBitRate;
pLinkDynPrm->interFrameInterval = 1;
pLinkDynPrm->mvAccuracy = IVIDENC2_MOTIONVECTOR_QUARTERPEL;
printf("pDynPrm->targetBitRate:%d ....\n", pDynPrm->targetBitRate);
printf("pDynPrm->inputFrameRate:%d ....\n", pDynPrm->inputFrameRate);
pLinkDynPrm->inputFrameRate = pDynPrm->inputFrameRate;
pLinkDynPrm->rcAlg = pDynPrm->rcAlg;
pLinkDynPrm->qpMin = pDynPrm->qpMin;
pLinkDynPrm->qpMax = pDynPrm->qpMax;
pLinkDynPrm->qpInit = pDynPrm->qpInit;
pLinkDynPrm->vbrDuration = pDynPrm->vbrDuration;
pLinkDynPrm->vbrSensitivity = pDynPrm->vbrSensitivity;

}
#endif
encPrm.inQueParams.prevLinkId = ipcInVideoId;
encPrm.inQueParams.prevLinkQueId = 0;
encPrm.outQueParams.nextLink = gVencModuleContext.ipcBitsOutRTOSId;


/* IPC Bits Out Video M3 link */
ipcBitsOutVideoPrm.baseCreateParams.inQueParams.prevLinkId = gVencModuleContext.encId;
ipcBitsOutVideoPrm.baseCreateParams.inQueParams.prevLinkQueId = 0;
ipcBitsOutVideoPrm.baseCreateParams.outQueParams[0].nextLink = gVencModuleContext.ipcBitsInHLOSId;
MultiCh_ipcBitsInitCreateParams_BitsOutRTOS(&ipcBitsOutVideoPrm, TRUE);

/* IPC Bits In Host link */
ipcBitsInHostPrm.baseCreateParams.inQueParams.prevLinkId = gVencModuleContext.ipcBitsOutRTOSId;
ipcBitsInHostPrm.baseCreateParams.inQueParams.prevLinkQueId = 0;
MultiCh_ipcBitsInitCreateParams_BitsInHLOS(&ipcBitsInHostPrm);

以下为LOG信息

pDynPrm->targetBitRate:2000000 ....
pDynPrm->inputFrameRate:30 ....
[m3vpss ] 10079: CAPTURE: Create in progress !!!
[m3vpss ] 10117: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!!
[m3vpss ] UTILS: DMA: Allocated CH (TCC) = 58 (58)
[m3vpss ] UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
[m3vpss ] UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
[m3vpss ] UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
[m3vpss ] UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
[m3video] 10289: IPC_IN_M3 : Create in progress !!!
[m3video] 10289: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3vpss ] CAPTURE::HEAPID:0 USED:328
[m3video] 10290: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3vpss ] CAPTURE::HEAPID:4 USED:29030400
[m3video] 10293: IPC_IN_M3 : Create Done !!!
[m3vpss ] 10280: CAPTURE: Create Done !!!
[m3video] 10293: ENCODE: Create in progress ... !!!
[m3vpss ] 10285: DUP: 0: Format: INTERLACED , 1920 x 1080
[m3vpss ] 10287: DUP : Create Done !!!
[m3vpss ] 10287: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 10289: IPC_OUT_M3 : Create Done !!!
[m3video] 10324: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1920, 1920) [INTERLACED ] [NON-TILED ], bitrate = 2000 Kbps, I-P Interval 1...
[m3video] 10417:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[576]::INTERNAL ERROR:-1
[m3video] ALGCONTROL FAILED:CMD:1
[m3video] ERROR: IH264ENC_LEVEL_INCOMPLAINT_PARAMETER , 0,
[m3video] 10417:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[587]::INTERNAL ERROR:0
[m3video] Ext Error :0
[m3video] EXT_ERROR: IH264ENC_EXTERROR_FRMRATE_NUMUNITSINTICKS = 37
[m3video] EXT_ERROR: IH264ENC_EXTERROR_LEVELLIMIT_RESOLUTION = 71

  • 你好;

          你是用的那个版本的sdk调试的?

  • ternence hsu 你好:

        我用的是V04.01

  • cheng li9 说:
    [m3vpss ] 10285: DUP: 0: Format: INTERLACED , 1920 x 1080

    这里的 interlaced 你可以去查一下,你caputre的格式是yuv420sp ,格式是没有问题的。

    cheng li9 说:
    [m3video] 10324: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1920, 1920) [INTERLACED ] [NON-TILED ], bitrate = 2000 Kbps, I-P Interval 1...
    [m3video] 10417:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[576]::INTERNAL ERROR:-1
    [m3video] ALGCONTROL FAILED:CMD:1
    [m3video] ERROR: IH264ENC_LEVEL_INCOMPLAINT_PARAMETER , 0,
    [m3video] 10417:!ERROR!:ENCLINK::links_m3video/iva_enc/encLink_h264.c:[587]::INTERNAL ERROR:0

    这里的错误你可以到 encLink_h264.c 的代码里面去查一下问题。

  • 问题已解决!谢谢

  • ternence hsu 你好!

        很感谢你的支持,之前那个问题已经解决,但是现在面临新的问题,我的输入源是1080P 逐行扫描60帧,但是经过dup给encode编码结束后成30帧了,明显比

    采集输入视频源慢,我通过Venc_setDynamicParam(0, 0, &params, VENC_FRAMERATE);将帧率设置为60帧后,编码出来的帧率达到了要求确实为60帧,但是

    编码出来的视屏图像比采集的源视频有快了。请问这是什么原因造成的?


  • 你好;

            你现在是编码为30帧,画面播放正常,如果编码为60帧,画面就快一倍,是这样吗?

           你的输入要源是60帧,应当是在某个模块丢帧了? 你检查一下你配置的模块的in , out 的帧率是不是都是配置一致,都是60帧处理的?

  • 你好!ternence hsu

    我的采集源是60帧的,本来是要编码成60帧,但编码出来成了30帧,显示比较慢不正常;

    prm_cap_inst->standard           = SYSTEM_STD_1080P_60;


  • 你好;

            你可以把dup 的第二路先关闭,只测试采集和编码,确定帧率是不是正常的;

            同时在 ti_vsys.c 里面有两个函数可以查看link 的工作状态,你看一下。

            Int32 Vsys_printDetailedStatistics()  和 Int32 Vsys_printBufferStatistics();

           

  • 你好:ternence hsu

        我把dup第二路关闭后编码出来的仍然是30帧,

        以下LOG是加了Vsys_printDetailedStatistics()  和 Int32 Vsys_printBufferStatistics();打出的信息

       这个说明我从VPSS M3采集输出的是51帧是吗?

    [m3vpss ]
    [m3vpss ] *** Capture List Manager Advanced Statistics ***
    [m3vpss ]
    [m3vpss ] List Post Count : 1
    [m3vpss ] List Stall Count : 0
    [m3vpss ] List Post Time (ms) : Max = 0, Min = 0, Avg = 0, Total = 0
    [m3vpss ] INTC Timeout Count : (0, 0) (Min timeout value = 994, 1000)
    [m3vpss ] Descriptor miss found count : 0
    [m3vpss ]
    [m3vpss ]
    [m3vpss ] VIP and VPDMA registers,
    [m3vpss ] VIP0 : FIQ_STATUS : 0x4810551c = 0x00000000
    [m3vpss ] VIP1 : FIQ_STATUS : 0x48105a1c = 0x00000000
    [m3vpss ] VPDMA: LIST_BUSY : 0x4810d00c = 0x00000000
    [m3vpss ]
    [m3vpss ]
    [m3vpss ] 6317: CAPTURE: Fields = 0 (fps = 0, CPU Load = 0)
    [m3vpss ] 6317: CAPTURE: Num Resets = 0 (Avg 0 ms per reset)
    [m3vpss ] 6318: SYSTEM : FREE SPACE : System Heap = 244336 B, Mbx = 10239 msgs)
    [m3vpss ] 6318: SYSTEM : FREE SPACE : SR0 Heap = 2129920 B (2 MB)
    [m3vpss ] 6318: SYSTEM : FREE SPACE : Frame Buffer = 76923776 B (73 MB)
    [m3vpss ] 6318: SYSTEM : FREE SPACE : Bitstream Buffer = 78690176 B (75 MB)
    [m3vpss ] TILER_STATS: CNT :8BIT
    [m3vpss ] TILER_STATS: CNT RESOLUTION: 16384 x 5440
    [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 16384 x 5436
    [m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
    [m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
    [m3vpss ] TILER_STATS: TOTAL FREE AREA: 89063424 (99 %)
    [m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
    [m3vpss ] TILER_STATS: CNT :16BIT
    [m3vpss ] TILER_STATS: CNT RESOLUTION: 32768 x 1344
    [m3vpss ] TILER_STATS: BUCKET RESOLUTION: 32768 x 1344
    [m3vpss ] TILER_STATS: NUM FREE BUCKETS: 1
    [m3vpss ] TILER_STATS: NUM USED BUCKETS: 0
    [m3vpss ] TILER_STATS: TOTAL FREE AREA: 44040192 (100 %)
    [m3vpss ] TILER_STATS: TOTAL USED AREA: 0 (0 %)
    [m3vpss ] 6320: SYSTEM : FREE SPACE : Tiler 8-bit = 89063424 B (84 MB) - TILER ON
    [m3vpss ] 6320: SYSTEM : FREE SPACE : Tiler 16-bit = 44040192 B (42 MB) - TILER ON
    [m3video] 12321: HDVICP-ID:0
    [m3video] All percentage figures are based off totalElapsedTime
    [m3video] totalAcquire2wait :1 %
    [m3video] totalWait2Isr :95 %
    [m3video] totalIsr2Done :0 %
    [m3video] totalWait2Done :95 %
    [m3video] totalDone2Release :0 %
    [m3video] totalAcquire2Release :97 %
    [m3video] totalAcq2acqDelay :2 %
    [m3video] totalElapsedTime in msec : 5947
    [m3video] numAccessCnt: 259
    [m3video] IVA-FPS : 51
    [m3video] Average time spent per frame in microsec: 21812
    [m3video] 12323: HDVICP-ID:1
    [m3video] All percentage figures are based off totalElapsedTime
    [m3video] totalAcquire2wait :0 %
    [m3video] totalWait2Isr :0 %
    [m3video] totalIsr2Done :0 %
    [m3video] totalWait2Done :0 %
    [m3video] totalDone2Release :0 %
    [m3video] totalAcquire2Release :0 %
    [m3video] totalAcq2acqDelay :0 %
    [m3video] totalElapsedTime in msec : 0
    [m3video] numAccessCnt: 0
    [m3video] IVA-FPS : 0
    [m3video] Average time spent per frame in microsec: 0
    [m3video] 12323: HDVICP-ID:2
    [m3video] All percentage figures are based off totalElapsedTime
    [m3video] totalAcquire2wait :0 %
    [m3video] totalWait2Isr :0 %
    [m3video] totalIsr2Done :0 %
    [m3video] totalWait2Done :0 %
    [m3video] totalDone2Release :0 %
    [m3video] totalAcquire2Release :0 %
    [m3video] totalAcq2acqDelay :0 %
    [m3video] totalElapsedTime in msec : 0
    [m3video] numAccessCnt: 0
    [m3video] IVA-FPS : 0
    [m3video] Average time spent per frame in microsec: 0
    [m3video]
    [m3video] *** ENCODE Statistics ***
    [m3video]
    [m3video] Elasped Time : 5 secs
    [m3video]
    [m3video]
    [m3video] CH | In Recv In Skip In User Out Latency
    [m3video] Num | FPS FPS Skip FPS FPS Min / Max
    [m3video] --------------------------------------------
    [m3video] 0 | 70 19 0 51 255 / 4503
    [m3video]
    [m3video] Multi Channel Encode Average Submit Batch Size
    [m3video] Max Submit Batch Size : 24
    [m3video] IVAHD_0 Average Batch Size : 1
    [m3video] IVAHD_0 Max achieved Batch Size : 1
    [m3video]
    [m3video] Multi Channel Encode Batch break Stats
    [m3video] Total Number of Batches created: 257
    [m3video] All numbers are based off total number of Batches created
    [m3video] Batch breaks due to batch sizeexceeding limit: 100 %
    [m3video] Batch breaks due to ReqObj Que being empty: 0 %
    [m3video] Batch breaks due to changed resolution class: 0 %
    [m3video] Batch breaks due to interlace and progressivecontent mix: 0 %
    [m3video] Batch breaks due to channel repeat: 0 %
    [m3video] Batch breaks due to different codec: 0 %
    [m3vpss ]
    [m3vpss ] 15327: LOAD: CPU: 4.9% HWI: 0.7%, SWI:1.2%
    [m3vpss ]
    [m3vpss ] 15327: LOAD: TSK: IPC_OUT_M30 : 0.6%
    [m3vpss ] 15327: LOAD: TSK: CAPTURE : 0.7%
    [m3vpss ] 15327: LOAD: TSK: MISC : 1.7%
    [m3vpss ]
    [m3video]
    [m3video] 15828: LOAD: CPU: 7.2% HWI: 0.8%, SWI:0.8%
    [m3video]
    [m3video] 15828: LOAD: TSK: IPC_IN_M30 : 0.7%
    [m3video] 15829: LOAD: TSK: IPC_BITS_OUT0 : 0.8%
    [m3video] 15829: LOAD: TSK: ENC0 : 2.1%
    [m3video] 15829: LOAD: TSK: ENC_PROCESS_TSK_0 : 1.5%
    [m3video] 15829: LOAD: TSK: MISC : 0.5%
    [m3video]
    [c6xdsp ]
    [c6xdsp ] 15950: LOAD: CPU: 0.2% HWI: 0.0%, SWI:0.0%
    [c6xdsp ]
    [c6xdsp ] 15950: LOAD: TSK: MISC : 0.2%
    [c6xdsp ]
    [HOST]
    ThreadName:IpcBitsOutLink_tskMain_30000018,ThreadID:300
    [m3vpss ]
    [m3vpss ] *** CAPTURE Statistics ***
    [m3vpss ] 16831: CAPTURE: Queued to driver = 632, Dequeued from driver = 628
    [m3vpss ] CAPTURE [0] Buf Q Status
    [m3vpss ] Empty Q -> count 0, wrPtr 0, rdPtr 0
    [m3vpss ] Full Q -> count 0, wrPtr 244, rdPtr 244
    [m3video]
    [m3video] *** Encode Statistics ***
    [m3video] 17332: ENC: Rcvd from prev = 658, Returned to prev = 655
    [m3video] ENC Out BitBuf Q Status
    [m3video] Empty Q 0 -> count 1, wrPtr 97, rdPtr 96
    [m3video] Full Q -> count 0, wrPtr 93, rdPtr 93

    这个说明我从VPSS M3采集输出的是51帧是吗?

  • 你好;

           你最好是跟一下每个link 的帧率,在link 中 的process 函数中,每帧数据加一个打印就出来了。

    • ternence hsu 你好!
    • 关于如何跟踪每个link的帧率我没找到相关process函数,能否以cap为例举个例子?谢谢