This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3359icev2 网卡问题



硬件平台:am3359icev2开发板

环境:ti-processor-sdk-linux-rt-am335x-evm-03.01.00.06-Linux-x86-Install

环境:busybox1.12.0

问题描述:

采用ti-processor-sdk-linux-rt-am335x-evm-03.01.00.06-Linux-x86-Install制作linux 内核,

采用busybox1.12.0编译简易文件系统

采用SD引导,能够进入系统,

但是,ifconfig时提示

ifconfig -a


lo Link encap:Local Loopback
LOOPBACK MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

sit0 Link encap:IPv6-in-IPv4
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

这是什么原因,为何不显示网卡信息???