目前在CCS6上验证 AM572X SDK中提供的Image Processing Demo,按照官方给出的教程运行代码后成功显示出AM572X EVM的IP(如下),然而在网页中输入对应IP却无法访问,网线均已正确连接,是否还需要其他设置?
[CortexA15_0] Using MAC Address: a4-d5-78-c4-f9-24
Using MAC Address: a4-d5-78-c4-f9-24
Service Status: DHCPC : Enabled : : 000
Service Status: HTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Enter Ipc_start
Ipc_start OK
Ipc_attach() OK
mc_process_init OK
ipc_heap_init OK
Network Added: If-1:192.168.65.103
Service Status: DHCPC : Enabled : Running : 017