This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于6678 cache的疑问



工程师你好:

最近看了6678的cache手册,仍有下面不确定的问题,请解答(以下都是说的数据cache,不是程序cache)。

1、CPU对L2 RAM和L2 Cache的访问速度是不是一样的?L2 Cache是不是只能缓存其他core的L2、EMIF、DDR3的空间,不能缓存本级的L2 RAM和SL2?

2、在程序刚开始运行时,对DDR3(DDR3已配置可Cache)的数据进行读操作,L1D和L2 Cache都是空的,L1D进行了相应空间的cache,那L2还会不会进行相应空间的cache,也就是同时备份数据?

3、若想invadite某个空间,不确定该空间是否在L1D或者L2中cache,是不是L1D和L2都要invadite?还是L1D invadite了,L2自动invadite?