This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

float类型数通过tms320c6xx汇编指令怎样输出,小数部分约去了,为什么?怎样解决?



请问一下例如float类型数y6=10.0在内存中的显示形式为0x41200000  (因为float数在内存中是IEEE754格式)

我用的是dsp的tms320c6xx汇编指令,计算4个float数的和,用的是c调用汇编模块,在汇编程序中通过计算将这个值y6放在了寄存器A4中,然后通过指令"B B3"将其输出,但输出y6不是10.4(0x41266666),而是10.0(0x41200000),小数部分约去了,为什么?怎样解决?

C程序如下:
int n6=4;
float y6=0;
float huibian_ys12[4]={11,2.1,3.1,4.1};
y6=ave6(huibian_ys12,n6);

汇编程序(ave6.asm)如下:
.global ave6
ave6:      MV.L2       B4,B1
             ZWRO.L1     A6
LOOP:    LDW.D1      *A4++,A2
             NOP          4
            ADDSP.L1    A2,A6,A6
            NOP          3
            SUB.S2       B1,1,B1
   [B1]   B.S2         LOOP
            NOP         5
            SHRU.S1      A6,0,A4      ;A4存放最终结果

            SPINT     A4,A4        ;浮点转int

            NOP        3
             B            B3
            NOP          5
            .end

 

  • 在ccs中显示数据时可以选择float,之后会显示浮点数据。你可以先直接用c语言实现几个浮点数的运算,结果存在浮点变量中,然后在ccs中查看数据值,确认是否你的汇编代码问题。