This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在c5509a上用mcbsp0和dma无法进dma中断



参考官方的csl例程中的dma4,将mcbsp1替换为mcbsp0后dma中断就无法进入了,数据搬移无法进行,不知什么原因?代码如下:

/*
* Copyright (C) 2003 Texas Instruments Incorporated
* All Rights Reserved
*/
/*
*---------main_dma4.c---------
* This example places the MCBSP in digital loopback mode and
* syncs MCBSP receive with DMA channel 4 and MCBSP transmit
* with DMA channel 5.
* The example uses predefined CSL macros and symbolic
* constants to create the initialization values needed for
* the MCBSP and DMA control registers to effect the transfer
*/
#include <stdio.h>

#include <csl_mcbsp.h>
#include <csl_dma.h>
#include <csl_irq.h>

//---------Global constants---------
#define N 128

//---------Global data definition---------

/* Define transmit and receive buffers */
#pragma DATA_SECTION(xmt,"dmaMem")
Uint16 xmt[N];
#pragma DATA_SECTION(rcv,"dmaMem")
Uint16 rcv[N];

MCBSP_Config ConfigLoopBack16= {
MCBSP_SPCR1_RMK(
MCBSP_SPCR1_DLB_ON, /* DLB = 1 */
MCBSP_SPCR1_RJUST_RZF, /* RJUST = 0 */
MCBSP_SPCR1_CLKSTP_DISABLE, /* CLKSTP = 0 */
MCBSP_SPCR1_DXENA_NA, /* DXENA = 0 */
MCBSP_SPCR1_ABIS_DISABLE, /* ABIS = 0 */
MCBSP_SPCR1_RINTM_RRDY, /* RINTM = 0 */
0, /* RSYNCER = 0 */
MCBSP_SPCR1_RRST_DISABLE /* RRST = 0 */
),
MCBSP_SPCR2_RMK(
MCBSP_SPCR2_FREE_NO, /* FREE = 0 */
MCBSP_SPCR2_SOFT_NO, /* SOFT = 0 */
MCBSP_SPCR2_FRST_FSG, /* FRST = 0 */
MCBSP_SPCR2_GRST_CLKG, /* GRST = 0 */
MCBSP_SPCR2_XINTM_XRDY, /* XINTM = 0 */
0, /* XSYNCER = N/A */
MCBSP_SPCR2_XRST_DISABLE /* XRST = 0 */
),
MCBSP_RCR1_RMK(
MCBSP_RCR1_RFRLEN1_OF(0), /* RFRLEN1 = 0 */
MCBSP_RCR1_RWDLEN1_16BIT /* RWDLEN1 = 5 */
),
MCBSP_RCR2_RMK(
MCBSP_RCR2_RPHASE_SINGLE, /* RPHASE = 0 */
MCBSP_RCR2_RFRLEN2_OF(0), /* RFRLEN2 = 0 */
MCBSP_RCR2_RWDLEN2_8BIT, /* RWDLEN2 = 0 */
MCBSP_RCR2_RCOMPAND_MSB, /* RCOMPAND = 0 */
MCBSP_RCR2_RFIG_YES, /* RFIG = 0 */
MCBSP_RCR2_RDATDLY_0BIT /* RDATDLY = 0 */
),
MCBSP_XCR1_RMK(
MCBSP_XCR1_XFRLEN1_OF(0), /* XFRLEN1 = 0 */
MCBSP_XCR1_XWDLEN1_16BIT /* XWDLEN1 = 5 */

),
MCBSP_XCR2_RMK(
MCBSP_XCR2_XPHASE_SINGLE, /* XPHASE = 0 */
MCBSP_XCR2_XFRLEN2_OF(0), /* XFRLEN2 = 0 */
MCBSP_XCR2_XWDLEN2_8BIT, /* XWDLEN2 = 0 */
MCBSP_XCR2_XCOMPAND_MSB, /* XCOMPAND = 0 */
MCBSP_XCR2_XFIG_YES, /* XFIG = 0 */
MCBSP_XCR2_XDATDLY_0BIT /* XDATDLY = 0 */
),
MCBSP_SRGR1_RMK(
MCBSP_SRGR1_FWID_OF(1), /* FWID = 1 */
MCBSP_SRGR1_CLKGDV_OF(1) /* CLKGDV = 1 */
),
MCBSP_SRGR2_RMK(
MCBSP_SRGR2_GSYNC_FREE, /* FREE = 0 */
MCBSP_SRGR2_CLKSP_RISING, /* CLKSP = 0 */
MCBSP_SRGR2_CLKSM_INTERNAL, /* CLKSM = 1 */
MCBSP_SRGR2_FSGM_DXR2XSR, /* FSGM = 0 */
MCBSP_SRGR2_FPER_OF(15) /* FPER = 0 */
),
MCBSP_MCR1_DEFAULT,
MCBSP_MCR2_DEFAULT,
MCBSP_PCR_RMK(
MCBSP_PCR_IDLEEN_RESET, /* IDLEEN = 0 */
MCBSP_PCR_XIOEN_SP, /* XIOEN = 0 */
MCBSP_PCR_RIOEN_SP, /* RIOEN = 0 */
MCBSP_PCR_FSXM_INTERNAL, /* FSXM = 1 */
MCBSP_PCR_FSRM_EXTERNAL, /* FSRM = 0 */
MCBSP_PCR_CLKXM_OUTPUT, /* CLKXM = 1 */
MCBSP_PCR_CLKRM_INPUT, /* CLKRM = 0 */
MCBSP_PCR_SCLKME_NO, /* SCLKME = 0 */
0, /* DXSTAT = N/A */
MCBSP_PCR_FSXP_ACTIVEHIGH, /* FSXP = 0 */
MCBSP_PCR_FSRP_ACTIVEHIGH, /* FSRP = 0 */
MCBSP_PCR_CLKXP_RISING, /* CLKXP = 0 */
MCBSP_PCR_CLKRP_FALLING /* CLKRP = 0 */
),
MCBSP_RCERA_DEFAULT,
MCBSP_RCERB_DEFAULT,
MCBSP_RCERC_DEFAULT,
MCBSP_RCERD_DEFAULT,
MCBSP_RCERE_DEFAULT,
MCBSP_RCERF_DEFAULT,
MCBSP_RCERG_DEFAULT,
MCBSP_RCERH_DEFAULT,
MCBSP_XCERA_DEFAULT,
MCBSP_XCERB_DEFAULT,
MCBSP_XCERC_DEFAULT,
MCBSP_XCERD_DEFAULT,
MCBSP_XCERE_DEFAULT,
MCBSP_XCERF_DEFAULT,
MCBSP_XCERG_DEFAULT,
MCBSP_XCERH_DEFAULT
};

/* Create DMA Receive Side Configuration */
DMA_Config dmaRcvConfig = {
DMA_DMACSDP_RMK(
DMA_DMACSDP_DSTBEN_NOBURST,
DMA_DMACSDP_DSTPACK_OFF,
DMA_DMACSDP_DST_DARAM,
DMA_DMACSDP_SRCBEN_NOBURST,
DMA_DMACSDP_SRCPACK_OFF,
DMA_DMACSDP_SRC_PERIPH,
DMA_DMACSDP_DATATYPE_16BIT
), /* DMACSDP */
DMA_DMACCR_RMK(
DMA_DMACCR_DSTAMODE_POSTINC,
DMA_DMACCR_SRCAMODE_CONST,
DMA_DMACCR_ENDPROG_ON,
DMA_DMACCR_REPEAT_OFF,
DMA_DMACCR_AUTOINIT_OFF,
DMA_DMACCR_EN_STOP,
DMA_DMACCR_PRIO_LOW,
DMA_DMACCR_FS_DISABLE,
DMA_DMACCR_SYNC_REVT1
), /* DMACCR */
DMA_DMACICR_RMK(
DMA_DMACICR_BLOCKIE_OFF,
DMA_DMACICR_LASTIE_OFF,
DMA_DMACICR_FRAMEIE_ON,
DMA_DMACICR_FIRSTHALFIE_OFF,
DMA_DMACICR_DROPIE_OFF,
DMA_DMACICR_TIMEOUTIE_OFF
), /* DMACICR */
(DMA_AdrPtr)(MCBSP_ADDR(DRR10)), /* DMACSSAL */
0, /* DMACSSAU */
(DMA_AdrPtr)&rcv, /* DMACDSAL */
0, /* DMACDSAU */
N, /* DMACEN */
1, /* DMACFN */
0, /* DMACFI */
0 /* DMACEI */
};

/* Create DMA Transmit Side Configuration */
DMA_Config dmaXmtConfig = {
DMA_DMACSDP_RMK(
DMA_DMACSDP_DSTBEN_NOBURST,
DMA_DMACSDP_DSTPACK_OFF,
DMA_DMACSDP_DST_PERIPH,
DMA_DMACSDP_SRCBEN_NOBURST,
DMA_DMACSDP_SRCPACK_OFF,
DMA_DMACSDP_SRC_DARAM,
DMA_DMACSDP_DATATYPE_16BIT
), /* DMACSDP */
DMA_DMACCR_RMK(
DMA_DMACCR_DSTAMODE_CONST,
DMA_DMACCR_SRCAMODE_POSTINC,
DMA_DMACCR_ENDPROG_ON,
DMA_DMACCR_REPEAT_OFF,
DMA_DMACCR_AUTOINIT_OFF,
DMA_DMACCR_EN_STOP,
DMA_DMACCR_PRIO_LOW,
DMA_DMACCR_FS_DISABLE,
DMA_DMACCR_SYNC_XEVT1
), /* DMACCR */
DMA_DMACICR_RMK(
DMA_DMACICR_BLOCKIE_OFF,
DMA_DMACICR_LASTIE_OFF,
DMA_DMACICR_FRAMEIE_ON,
DMA_DMACICR_FIRSTHALFIE_OFF,
DMA_DMACICR_DROPIE_OFF,
DMA_DMACICR_TIMEOUTIE_OFF
), /* DMACICR */
(DMA_AdrPtr)&xmt[1], /* DMACSSAL */
0, /* DMACSSAU */
(DMA_AdrPtr)(MCBSP_ADDR(DXR10)), /* DMACDSAL */
0, /* DMACDSAU */
N, /* DMACEN */
1, /* DMACFN */
0, /* DMACFI */
0 /* DMACEI */
};

/* Define a DMA_Handle object to be used with DMA_open function */
DMA_Handle hDmaRcv, hDmaXmt;

/* Define a MCBSP_Handle object to be used with MCBSP_open function */
MCBSP_Handle hMcbsp;

volatile Uint16 transferComplete = FALSE;
Uint16 err = 0;
Uint16 old_intm;
Uint16 xmtEventId, rcvEventId;

//---------Function prototypes---------
/* Reference start of interrupt vector table */
/* This symbol is defined in file, vectors.s55 */
extern void VECSTART(void);

/* Protoype for interrupt functions */
interrupt void dmaXmtIsr(void);
interrupt void dmaRcvIsr(void);
void taskFxn(void);

//---------main routine---------
void main(void)
{
Uint16 i;

/* Initialize CSL library - This is REQUIRED !!! */
CSL_init();

/* Set IVPD/IVPH to start of interrupt vector table */
IRQ_setVecs((Uint32)(&VECSTART));

for (i = 0; i <= N - 1; i++) {
xmt[i] = i + 1;
rcv[i] = 0;
}

/* Call function to effect transfer */
taskFxn();
}

void taskFxn(void)
{
Uint16 srcAddrHi, srcAddrLo;
Uint16 dstAddrHi, dstAddrLo;
Uint16 i;

/* By default, the TMS320C55xx compiler assigns all data symbols word */
/* addresses. The DMA however, expects all addresses to be byte */
/* addresses. Therefore, we must shift the address by 2 in order to */
/* change the word address to a byte address for the DMA transfer. */
srcAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) >> 15) & 0xFFFFu;
srcAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) << 1) & 0xFFFFu;
dstAddrHi = (Uint16)(((Uint32)(&rcv)) >> 15) & 0xFFFFu;
dstAddrLo = (Uint16)(((Uint32)(&rcv)) << 1) & 0xFFFFu;

dmaRcvConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
dmaRcvConfig.dmacssau = srcAddrHi;
dmaRcvConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
dmaRcvConfig.dmacdsau = dstAddrHi;

srcAddrHi = (Uint16)(((Uint32)(&xmt[0])) >> 15) & 0xFFFFu;
srcAddrLo = (Uint16)(((Uint32)(&xmt[0])) << 1) & 0xFFFFu;
dstAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) >> 15) & 0xFFFFu;
dstAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) << 1) & 0xFFFFu;

dmaXmtConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
dmaXmtConfig.dmacssau = srcAddrHi;
dmaXmtConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
dmaXmtConfig.dmacdsau = dstAddrHi;

/* Open MCBSP Port 1 and set registers to their power on defaults */
hMcbsp = MCBSP_open(MCBSP_PORT0, MCBSP_OPEN_RESET);

/* Open DMA channels 4 & 5 and set regs to power on defaults */
hDmaRcv = DMA_open(DMA_CHA4,DMA_OPEN_RESET);
hDmaXmt = DMA_open(DMA_CHA5,DMA_OPEN_RESET);

/* Get interrupt event associated with DMA receive and transmit */
xmtEventId = DMA_getEventId(hDmaXmt);
rcvEventId = DMA_getEventId(hDmaRcv);

/* Temporarily disable interrupts and clear any pending */
/* interrupts for MCBSP transmit */
old_intm = IRQ_globalDisable();

/* Clear any pending interrupts for DMA channels */
IRQ_clear(xmtEventId);
IRQ_clear(rcvEventId);

/* Enable DMA interrupt in IER register */
IRQ_enable(xmtEventId);
IRQ_enable(rcvEventId);

/* Set Start Of Interrupt Vector Table */
IRQ_setVecs(0x10000);

/* Place DMA interrupt service addresses at associate vector */
IRQ_plug(xmtEventId,&dmaXmtIsr);
IRQ_plug(rcvEventId,&dmaRcvIsr);

/* Write values from configuration structure to MCBSP control regs */
MCBSP_config(hMcbsp, &ConfigLoopBack16);

/* Write values from configuration structure to DMA control regs */
DMA_config(hDmaRcv,&dmaRcvConfig);
DMA_config(hDmaXmt,&dmaXmtConfig);

#if 0
/* Take MCBSP transmit and receive out of reset */
MCBSP_start(hMcbsp,
MCBSP_XMIT_START | MCBSP_RCV_START,
0u);

/* Prime MCBSP DXR */
while (!(MCBSP_xrdy(hMcbsp))){
;
}
MCBSP_write16(hMcbsp,xmt[0]);

/* Enable all maskable interrupts */
IRQ_globalEnable();

/* Enable DMA */
DMA_start(hDmaRcv);
DMA_start(hDmaXmt);

/* Start Sample Rate Generator and Enable Frame Sync */
MCBSP_start(hMcbsp,
MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
0x300u);
#else
/* Enable all maskable interrupts */
IRQ_globalEnable();

/* Start Sample Rate Generator and Enable Frame Sync */
MCBSP_start(hMcbsp,
MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
0x300u);

/* Enable DMA */
DMA_start(hDmaRcv);
DMA_start(hDmaXmt);

/* Take MCBSP transmit and receive out of reset */
MCBSP_start(hMcbsp,
MCBSP_XMIT_START | MCBSP_RCV_START,
0u);
#endif
/* Wait for DMA transfer to be complete */
while (!transferComplete){
;
}

/*------------------------------------------*\
* Compare values
\*------------------------------------------*/
for(i = 0; i <= N - 1; i++){
if (rcv[i] != xmt[i]){
++err;
break;
}
}

printf ("%s\n",err?"TEST FAILED" : "TEST PASSED");

/* Restore status of global interrupt enable flag */
IRQ_globalRestore(old_intm);

/* We're done with MCBSP and DMA , so close them */
MCBSP_close(hMcbsp);
DMA_close(hDmaRcv);
DMA_close(hDmaXmt);
}

interrupt void dmaXmtIsr(void) {
DMA_stop(hDmaXmt);
IRQ_disable(xmtEventId);
}

interrupt void dmaRcvIsr(void) {
DMA_stop(hDmaRcv);
IRQ_disable(rcvEventId);
transferComplete = TRUE;
}

/////下面是vectors_dma4.s55的内容未修改

*
* Copyright (C) 2003 Texas Instruments Incorporated
* All Rights Reserved
*
*
*---------vectors_dma4.s55---------
*
* Assembly file to set up interrupt vector table
*

.sect ".vectors"

*------------------------------------------------------------------------------
* Global symbols defined here and exported out of this file
*------------------------------------------------------------------------------

.global _VECSTART

*------------------------------------------------------------------------------
* Global symbols referenced in this file but defined somewhere else.
* Remember that your interrupt service routines need to be referenced here.
*------------------------------------------------------------------------------
.ref _c_int00

.def nmi, int0, int1, int2, int3, int4, int5, int6
.def int7, int8, int9, int10, int11, int12, int13
.def int14, int15, int16, int17, int18, int19, int20
.def int21, int22, int23, int24, int25, int26, int27
.def int28, int29

_VECSTART:
.ivec _c_int00,use_reta
nmi .ivec no_isr
nop_16
int0 .ivec no_isr
nop_16
int1 .ivec no_isr
nop_16
int2 .ivec no_isr
nop_16
int3 .ivec no_isr
nop_16
int4 .ivec no_isr
nop_16
int5 .ivec no_isr
nop_16
int6 .ivec no_isr
nop_16
int7 .ivec no_isr
nop_16
int8 .ivec no_isr
nop_16
int9 .ivec no_isr
nop_16
int10 .ivec no_isr
nop_16
int11 .ivec no_isr
nop_16
int12 .ivec no_isr
nop_16
int13 .ivec no_isr
nop_16
int14 .ivec no_isr
nop_16
int15 .ivec no_isr
nop_16
int16 .ivec no_isr
nop_16
int17 .ivec no_isr
nop_16
int18 .ivec no_isr
nop_16
int19 .ivec no_isr
nop_16
int20 .ivec no_isr
nop_16
int21 .ivec no_isr
nop_16
int22 .ivec no_isr
nop_16
int23 .ivec no_isr
nop_16
int24 .ivec no_isr
nop_16
int25 .ivec no_isr
nop_16
int26 .ivec no_isr
nop_16
int27 .ivec no_isr
nop_16
int28 .ivec no_isr
nop_16
int29 .ivec no_isr
nop_16

*------------------------------------------------------------------------------
* This is a dummy interrupt service routine used to initialize the IST.
*------------------------------------------------------------------------------
.text
.def no_isr
no_isr:
b #no_isr
*------------------------------------------------------------------------------