This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 EMIF接NOR Flash的疑问



最近做c6678通过emif接口外接S29GL01GS  norflash并使其做为boot加载程序,碰到如下疑问:
1.硬件设计说明6.11.1节描述的boot时从CS2的基地址运行程序,这是指DSP上EMIF接口的片选CE2吗?是不是说dsp的CE2要接S29GL01GS11DHIV10的片选引脚?
2.DSP上emif只有24跟地址线,16根数据线,每个片选对应的大小应该为2^24x16/2 = 32MB,为什么EMIF手册上说的是64MB?
3. DSP上EMIF接口的wait0和wait1信号做什么用的,flash上没有对应的信号与之相连,这个该怎么接?
4.S29GL01GS11DHIV10是128MB的flash,那不是要接到DSP的多个片选脚,这个flash的片选脚和6678怎么接才正确?