This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.2连接DM36X EVM问题.



为什么CCS5.2总是无法连接到EVM呢? 能帮忙看看是什么问题么?

  • 图片看不清把  这是文字

    ARM9: GEL Output:

    DM365EVM ARM Startup Sequence

    ARM9: GEL Output: VPSS Sync Reset Fix

    ARM9: GEL: Error while executing OnTargetConnect(): Target failed to write memory at 0x01C21C0C at *((unsigned int *) 0x01C21C0C)=0x00020002 [evmdm365.gel:104] at OnTargetConnect() .

    ARM9: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.681.0)

    ARM9: Failed Software Reset

    ARM9: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.681.0)

    ARM9: GEL Output: Disable VPSS

    ARM9: GEL: Error calling OnPreFileLoaded(): execution state prevented access at *((unsigned int *) 0x01C71000)=0 [evmdm365.gel:318] at Disable_VPSS() [evmdm365.gel:138] at OnPreFileLoaded()

    ARM9: GEL: File: C:\ti\workspace_v5_2\DM365_LED\Debug\DM365_LED.out: Load failed.