This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't find a source file at "/tmp/TI_MKLIB4kQNZn/SRC/exit.c"



开发环境为CCS6.1,C5535加外部SPI FLASH,仿真正常,现在想把程序烧到外部flash里,采用了官网提供的TI SPI Flash Programmer和SPI Boot Files发现都无法完成下载,程序提示以下错误,求大神解救,out文件已转换为bin文件。

Can't find a source file at "/tmp/TI_MKLIB4kQNZn/SRC/exit.c"
Locate the file or edit the source lookup path to include its location.

  • 你把SPI Boot Files在ccs6.1重新编译一下再加载新的.out试试。

  • 肯定是编译过的,换了ccs5.5,一样的操作,还是一样的错误。。。

  • 那忽略这个错呢,看数据写到flash里了没?

  • 忽略过,然后断电上电看有没有运行程序,发现没有,好像是没有烧进去。
  • 用仿真器看一下flash里的内容是否是你烧进去的代码?

  • 这个如何查看呢,我flash是外部的,用的spiflash_write程序下载的。
  • 是SPI flash,那看不了。

    那只能连上仿真器,跟一下boot过程,看代码有没有加载进来?

  • 程序没运行,可能是你的程序有问题。

    spiflash_writer主函数main最后没有while(1),运行完后自然就进入exit.c退出了。上面根本就不是什么错误。

    void main( void )

    {
    /* Initialize BSL */
    EZDSP5535_init( );

    /* Display test ID */
    printf( "\nRunning SPI FLASH Writer...\n");

    /* Call test function */
    TestFail = spiflash_writer( );

    /* Check for test fail */
    if ( TestFail != 0 )
    {
    /* Print error message */
    printf( " FAIL... error code %d... quitting\n", TestFail );
    }
    else
    {
    /* Print pass message */
    printf( " PASS\n" );
    printf( "\n***ALL Tests Passed***\n" );
    }

    StopTest();
    }

    而spiflash_writer函数里回读校验,又怎么会没有写进去。

    Int16 spiflash_writer( )
    {
    Uint32 i, j, pages;
    Uint16* pdata;
    Int32 fileSize = 0;
    FILE *fPtr;
    Uint16 *ramPtr;

    /* Read the filename from host */
    printf("Enter the file Name:\r\n");
    scanf("%s", fileName);
    fflush(stdin);

    /* Open a File from the hard drive */
    printf("Opening file...\r\n");
    fPtr = fopen(fileName, "rb");
    if(fPtr == NULL)
    {
    printf("ERROR: File %s Open failed\r\n", fileName);
    return 1;
    }
    fileSize = 0; // Initialize size to 0

    /* Get file size */
    fseek(fPtr,0,SEEK_END);
    fileSize = ftell(fPtr);

    /* Setup pointer in RAM for temporary storage of data */
    ramPtr = (Uint16*) bootImage;

    if(fileSize == 0) // Check if file was found
    {
    printf("ERROR: File read failed.. Closing program.\r\n");
    fclose (fPtr);
    return 1;
    }
    fseek(fPtr,0,SEEK_SET);

    if (fileSize != fread(ramPtr, 1, fileSize, fPtr)) // Read file to ram and check if read properly
    {
    printf("WARNING: File Size mismatch.\r\n");
    return 1;
    }
    fseek(fPtr,0,SEEK_SET);

    /* Calculate number of pages */
    pages = (fileSize / spiflash_PAGESIZE) + 1;

    /* Initialize the SPI interface */
    EZDSP5535_SPIFLASH_init( );

    /* Erase target area in spiflash */
    printf("Erasing target area...\r\n");
    EZDSP5535_SPIFLASH_erase( 0, fileSize);

    /* Write to SPIFLASH */
    printf("Writing file...\r\n");
    for ( i = 0 ; i < pages ; i++ )
    {
    /* Write a page */
    EZDSP5535_SPIFLASH_write( ((Uint32)bootImage + (i * spiflash_PAGESIZE)), i * spiflash_PAGESIZE, spiflash_PAGESIZE );
    }

    /* Read and verify SPIFLASH */
    printf("Checking file...\r\n");
    for ( i = 0 ; i < pages ; i++ )
    {
    /* Read a page */
    EZDSP5535_SPIFLASH_read( i * spiflash_PAGESIZE, ( Uint32 )rx, spiflash_PAGESIZE );

    /* Check the pattern */
    pdata = ( Uint16* )((Uint32)bootImage + (i * spiflash_PAGESIZE));
    for ( j = 0 ; j < spiflash_PAGESIZE; j++ )
    {
    if ( ((*pdata++) & 0xFF)!= (rx[j]))
    return 1; // Fail
    }
    }
    return 0;

  • 1.console窗口打印出all tests passed是不是说明程序已经下载进去了? 2.仿真运行的时候管脚有输出,但是断电启动,管脚还是没有输出,我的程序是否有问题? 3.示波器上看到上电时spiclk上有5个字节加6个字节的clk信号,是否为boot信号,但是之后就没有了,5535没有去从flash里读程序? 4.5535是否有硬件管脚设置让其进入spiflash boot模式? 5.谢谢各位大神的耐心解答。
  • Hu Schuman 说:
    1.console窗口打印出all tests passed是不是说明程序已经下载进去了?

    理论上是的。

    Hu Schuman 说:
    3.示波器上看到上电时spiclk上有5个字节加6个字节的clk信号,是否为boot信号,但是之后就没有了,5535没有去从flash里读程序?

    说明芯片bootloader有去读flash, 但是没有完成,是不是你的bin文件转换的不对啊。你是怎么转的?

    Hu Schuman 说:
    4.5535是否有硬件管脚设置让其进入spiflash boot模式?

    不需要,C5535是按顺序从boot外设读关键字的,读到关键字才继续从该外设读数据。

  • bin文件按照你们提供的hex55转的,先修改demo.cmd,然后用cmd运行hex55将out转成bin的
  • 1.今天继续调试了下,发现SPICLK有5个字节加6个字节应该是尝试读16位SPI(5个字节)和尝试24位SPI(6个字节)是吗?

    2.16位的不管,我用的是24位的,从spiflash_write里看出下载到FLASH里的bootImage第0位为0x00,第1位为0x02,然后从6个字节的波形图里来看,确实读到了0x00 0x02(6个字节具体为0x03 0x00 0x00 0x00 0x00 0x02),然后就没有然后了,关键字是从地址0开始的2个字节吗?按理说5535应该继续往下读吧?求大神解答下,小弟感激不尽。