刚开始接触tmdxice3359这个板子,
1.安装了官网的SDK套件
2.并使用SDK套件中的create_sdcare.sh制作好了SD卡
3.并将接线帽的P2,P3连接在一起了,但是还是遇到了如下的问题:
并没有在串口中看到信息,只看到LED上显示了:Led App等信息。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
刚开始接触tmdxice3359这个板子,
1.安装了官网的SDK套件
2.并使用SDK套件中的create_sdcare.sh制作好了SD卡
3.并将接线帽的P2,P3连接在一起了,但是还是遇到了如下的问题:
并没有在串口中看到信息,只看到LED上显示了:Led App等信息。
因为是刚接触这个板子,有很多不熟悉的地方。可否给出烧写Flash的工具名称和下载链接?麻烦你了。
AM335X FLASH有几种烧写方法。
1,通过CCS JTAG来烧写。
http://processors.wiki.ti.com/index.php/AM335x_CCS_Flashing_Tools_Guide
2,通过USB/ETHERNET烧写。
3,先烧写在贴。(一般大量生产的时候使用)
方法1,需要JTAG仿真器,你们应该有TI的仿真器,XDS100 XDS560都可以,和DSP 是通用的。
方法2,不需要工具,有USB线或者网线就行。
请问你是跑什么操作系统?RT Linux?
现在用CCS7.1新建了一个简单工程,使用板载的XDS100V2仿真器无法连接芯片。仿真器测试测试正常,debug是提示
Error connecting to the target:
(Error -1266 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 6.0.576.0)
你先看看能否通过这个方式对SPI Flash进行擦除。