大家好:
1、 AM335x数据手册上VDD_CORE电压范围是(1.056V—1.144V ),请教一下这个电压范围是怎么得来的?
2、我用AM3352+TPS65910A3A1,主频1GHz,实测VDD_CORE电压普遍偏高,有时会有1.143V,非常接近范围上限了。如果加上万用表误差或PCB板本身误差,这个电压就会超限,有时会测得1.1465>1.144V,电压超限会怎样?VDD_CORE电压误差是±4%(其他电压误差±5%,VDD_MPU误差±8%),VDD_CORE的精度要求这么高?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1,这个电压范围是芯片出场决定的
2,不要超过上限,否则可能会影响芯片寿命。
VDD_CORE电压高出范围在误差之内是可以接受的,但是不能高出太多。
根据datasheet的table 5-1,压力测试下的极限电压是1.5V,超过这个电压,芯片肯定会永久损坏。
5.5的推荐是,在这个电压范围,能保证芯片的正常工作。如果超过了,不能100%保证芯片能正常工作。
你们用的什么PMU?在什么情况下会出现1.1465V的情况?
找到原因了,这个电压程序里本来就设置的1.137,有些偏高了,可以以12.5mv为单位调整。
在Uboot的时候, 我记得默认是设置为 1.1375的电压的,
tps65910_voltage_update(CORE, TPS65910_OP_REG_SEL_1_1_3)// 1.1375
这个是可以的,但是为什么你说偏高了呢