最近研究AM5728的PCIe,有些疑问没有搞明白,正好看到网上也有人问,就复制过来,看看TI的兄弟能不能帮忙解答一下。
I want to understand the usage of BARs in the PCIe Root Complex. The PCIe Root Complex is already a part of the CPU (as a peripheral to it). And the CPU register spaces is easily accessible. CPU has register to access its various peripheral link PCIe controller, DIMM Controller, USB Controllers etc. So in this case what is the usage of BAR inside the PCIe RC Config space ?
Secondly I want to understand how the PCIe RC is setup during enumeration with the proper memory windows. For example lets say I have a PCIe device (EP) directly connected to the RC. And in the Config space of EP programmed with some address 'X' with some size 's'. So basically, any read/write from the CPU to the window of 'X' and 'X +s', should go to the PCIe EP. But this should go through the PCIe RC. Now how the RC knows that it should it should translate the CPU read/write to that memory window into PCIe transaction to the EP ? How does the RC is configured to do that ? Are there any standardized register in PCIe RC where this information is kept ?